This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2652 would be no response after it scan several times

Part Number: CC2652R


Tool/software:

SDK version: 7.40.00.77

#!/bin/sh
#/usr/bin/blescan.sh
tty="$(uci -q get tisbl.tisbl.tty)"
[ -z "$tty" ] && tty='/dev/ttyMSM1'
exec 100>"/var/lock/ble.lock"
flock 100

MAX_COUNT=20
count=1

com-wr.sh "$tty" 3 "\x01\x1D\xFC\x01\x00" > /dev/null # this reset command delay time must >= 3, if small than 3, the following commands  will be something wrong
com-wr.sh "$tty" 1 "\x01\x00\xFE\x08\x02\x00\x00\x00\x00\x00\x00\x00" > /dev/null
com-wr.sh "$tty" 1 "\x01\x60\xFE\x04\x01\x00\x20\x00" > /dev/null
com-wr.sh "$tty" 1 "\x01\x60\xFE\x04\x01\x01\x20\x00" > /dev/null
com-wr.sh "$tty" 1 "\x01\x61\xFE\x02\x01\x02" > /dev/null
com-wr.sh "$tty" 1 "\x01\x61\xFE\x02\x01\x03" > /dev/null 
com-wr.sh "$tty" 1 "\x01\x61\xFE\x02\x01\x04" > /dev/null
com-wr.sh "$tty" 1 "\x01\x61\xFE\x02\x01\x05" > /dev/null 
#com-wr.sh "$tty" 3 "\x01\x51\xFE\x06\x00\x00\xF4\x01\x28\x00" | tee /tmp/blescan.data | ble-scan-rx-parser.sh

while [ $count -le $MAX_COUNT ]
do
	com-wr.sh "$tty" 10 "\x01\x51\xFE\x06\x00\x00\x00\x04\x00\x02" | tee /tmp/blescan.data | ble-scan-rx-parser.sh
	com-wr.sh "$tty" 1 "\x01\x52\xFE\x00" > /dev/null

	count=$((count + 1))
done

exec 100>&-


This attached code is how we send commands to CC2652 per scan cycle.

#!/bin/sh
# com-wr.sh tty time command parser
# example com-wr.sh /dev/ttyMSM1 1 "\x01\x1D\xFC\x01\x00" | hexdump.sh  --> send "\x01\x1D\xFC\x01\x00" to /dev/ttyMSM1 and then hexdump receive data until 100ms timeout
#command example "\x7E\x03\xD0\xAF und normaler Text" 
usleep 10000
tty=$1
time=$2
command=$3
parser=$4
stty -F $tty time $time 
exec 99< $tty
echo -en $command > $tty
cat $tty
exec 99<&-

This attached code is how we send commands to tty.

In current situation, we send command "\x01\x51\xFE\x06\x00\x00\x00\x04\x00\x02" via UART to make CC2652R scan BLE data.

After we repeat this action several times (about 6000 times), the CC2652R would be no response.

We would like to know that if there is any limit of scan times or what the root cause is.