Part Number: CC2640R2F
Tool/software:
I have a XDS110 emulator and a custom-made board that uses a CC2640R2F, the debug port is 2-wire cJTAG.
When I connect the emulator to my PC(Windows 11) it shows up in device manager, and was able to be identified by CCS 20.
However when I tried to create a "project-zero" and check the connection I got -242 error, which states "a router subpath could not be accessed".
I also tried IAR, and got same errors (the error should be returned by the device driver, both IDEs are just talking to the driver)
Here I have two questions:
1) I want to isolate the problem, does this error means the XDS110 is buggy, or the target board is buggy? I checked the connections they looked fine.
2) SmartRF programmer 2 cannot identify CC2640R2F as well. What should I do next to see what's going on? (I don't have any launchpads around so I cannot cross-compare).
Thanks!