This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2340R5: How to implement OAD in central Role

Part Number: CC2340R5


Tool/software:

Hi,

I am using the CC2340R5 device in central mode, but I need to implement the OAD feature in the central mode device. We have already implemented OAD in peripheral mode.

Is it possible to implement the OAD feature in central mode, or do we need to make it peripheral + central?

Please let me know if this is possible.

If it is possible, could you please provide documentation on how to implement it?"

Let me know if this works for you or if you need any further revisions!

SDK: simplelink_lowpower_f3_sdk_7_40_00_64

CCS: 12.5

Thanks, and regards 

Balaji Wankhede

  • Hi Balaji,

    The OAD examples provided in the F3 SDK assume the peripheral device will ask as the OAD target and a central will ask as the distributor. I would recommend running the project in peripheral + central when an OAD operation is to be performed as this will allow you to leverage all of the OAD resources and example code available in the SDK.

    Best Regards,

    Jan