This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2340R5: If CC2340R5 is working in dual mode (i.e., both central and peripheral mode) then can it connect with a central device as a peripheral and with a peripheral device as a central at the same time?

Part Number: CC2340R5

Tool/software:

I am using a CC2340R5 in a 2W TCU (Telematics control unit), it is working in dual mode i.e., Central and Peripheral both. I have a BLE keyfob which is working in peripheral mode and mobile phone working in a central mode. In my application there will be scenarios where keyfob and mobile phone both will be connected to TCU working is dual mode. So, i want to know is this possible to achieve. Can a device working in dual mode can be connected to devices (one working in peripheral mode and other working in central mode) at the same time.