Part Number: CC2340R5
Tool/software:
Hi TI Support Team,
I am planning to flash the CC2340 using the ROM serial bootloader over the SPI interface.
My setup includes two CC2340 MCUs: one acting as the host and the other as the slave.
According to TRM section 8.5, I have configured the SPI format with SPH set to 1, SPO set to 1, and a bit rate of 100k.
Additionally, I have set a host GPIO as an output to pull down the slave's DIO21, ensuring it enters bootloader mode.
The host sends the ping command (0x03 0x20 0x20) to the slave. However, I am unsure how to receive an acknowledgment from the slave.
I attempted to send a 512-byte SPI packet (including the ping command) to the slave, but I did not receive any acknowledgment data on MISO.
Could you provide guidance on properly using the ROM serial bootloader over SPI?
Thank you for your support.