Part Number: CC2745R10-Q1
Tool/software:
Dear Experts,
The following is the schematic diagram of CC2745.
Please help review whether the peripheral schematic design and ANT schematic design of CC2745 need to be optimized. Additionally, we have some questions regarding the design and hope to receive answers. Thank you very much
1. If CC2745 is used as a slave, which pins can be used as INT/WAKUP function pins
2. Is it necessary to reserve a reset circuit externally when using CC2745 as an MCU
3. For the convenience of subsequent debugging, which pins are recommended to reserve test points