Part Number: CC2340R5
Other Parts Discussed in Thread: UNIFLASH
Tool/software:
Hi Experts,
Greetings!
I have a question regarding firmware programming and RSSI testing during production for CC2340R5.
Currently, we are using UniFlash PC software along with the XDS110 Programmer to flash firmware onto our custom hardware. However, we are looking for a more efficient solution to speed up the mass production process.
Production Setup Details:
- Our custom hardware is arranged in a panel of 32 modules (8×4 matrix).
- Each module has SWD, UART, Power, GND, and Reset pins exposed, which can be utilized for programming and testing.
- Current Programming Time: It takes ~14 seconds to flash a single module using UniFlash (firmware size: 512KB).
- Target Requirement: We need to flash and read RSSI with respect to reference module for the entire 32-module panel within 60 seconds.
Could you please guide us on suitable hardware and software tools that can help us achieve this target and optimize our programming workflow for high-volume production?
Looking forward to your insights..
Best Regards,
HARINDER SINGH