Other Parts Discussed in Thread: SYSCONFIG
Tool/software:
Hi all,
I am testing basic BLE project using simplelink_lowpower_f3_sdk_8_40_00_61 on the cc2745 Launchpad.
I am attempting to modify the TX power during runtime by utilizing the HCI_EXT_SetTxPowerDbmCmd() function.
I have updated the TX power settings in SysConfig as shown below:

Additionally, I am using characteristic 1 of the Simple GATT Service in the Basic BLE project to send commands to change the TX power value during runtime. Below are my code snippets:
/********* changes in app_simple_gatt.c file*******************/
static void SimpleGatt_changeCB( uint8_t paramId )
{
int8_t newValue = 0;
switch( paramId )
{
case SIMPLEGATTPROFILE_CHAR1:
{
SimpleGattProfile_getParameter( SIMPLEGATTPROFILE_CHAR1, &newValue );
// Print the new value of char 1
MenuModule_printf(APP_MENU_PROFILE_STATUS_LINE, 0, "Profile status: Simple profile - "
"Char 1 value = " MENU_MODULE_COLOR_YELLOW "%d " MENU_MODULE_COLOR_RESET,
newValue);
if((newValue<=10) & (newValue>=-10))
{
set_txpower=1;
txpower_value=newValue;
}
}
break;
//.................//
}
/*************** app_simple_gatt.c*************/
/*************** custom task created to change tx power value*************/
void *SystemThread(void *arg0)
{
/* 1 second delay */
uint32_t time = 1;
// so that the application can send and receive messages.
ICall_registerApp(&selfEntityloc_sys, &syncEventloc_sys);
/* Call driver init functions */
GPIO_init();
// I2C_init();
// SPI_init();
// Watchdog_init();
while (1)
{
sleep(time);
GPIO_toggle(CONFIG_GPIO_LED_RED);
if(set_txpower)
{
set_txpower=0;//clear tx power flag
GAP_TerminateLinkReq(0, HCI_DISCONNECT_REMOTE_USER_TERM); //terminate connection
usleep(100000);
stop_adv(); //stop adv
usleep(100000);
HCI_EXT_SetTxPowerDbmCmd(txpower_value,0); //change tx power
MenuModule_printf(9, 0,"tx power changed to %d",txpower_value);
start_adv(); //start adv
}
}
}
But I am not able change the TX power using above code.
Please provide me the solution to resolve this issue.
Regards,
Aslam