Part Number: CC2755R10
Tool/software:
Hi team,
Customer is evaluating CC2755. They ask if SBL (Loading FW from Linux host via UART) can work on cc2755's bootloader. If not yet, what is the timeline you will add this to cc2755?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Jerry,
There is likely a large amount of reuse available from the TI_CC2340_Linux_SBL solution, with the same CCFG address and serial ROM bootloader command layer, but there will be some changes required to sbl_device_cc2340.c/h based on assumptions around a 512 kB flash memory and 36 kB RAM. I will loop in another expert to comment on upcoming F3 device SBL Linux host development.
Regards,
Ryan
There is not currently a timeline for CC2755 SBL Linux host tool release.
Regards,
Ryan