Part Number: CC2640R2F
Tool/software:
Im trying to set one of the DIO pins on a custom board with the CC2640R2F microcontroller as an output pin in the tri-state mode. In the technical reference manual, it says that (page 989) "By disabling the output buffer the corresponding I/O pin will be in the tri-state condition (high impedance). If nothing is driving the I/O to a valid logical level when the output buffer is disabled then disable the input buffer to avoid excessive current draw through the I/O input buffer." How exactly are the output and input buffers enabled/disabled?