This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2340R5: Problem flashing a blank device with Segger J-Link

Part Number: CC2340R5
Other Parts Discussed in Thread: UNIFLASH

Tool/software:

Dear TI team,

We are having devices with the CC2340R5 MCU for Bluetooth functionality and they should be coming blank from the factory. Yesterday I tried to flash a blank CC2340R5 through Segger J-Link, but it failed as it failed to erase the memory. Then I flashed the device by using Uniflash and a XDS110 debugger and after that I had no problems doing the flashing with the J-Link. My questions are - could you give me any idea why the initial flash through J-Link? Why did it fail to erase the memory? Can I fix this and how? I'm attaching a log from J-Link and the CCFG (in Intel HEX format) of the blank device.

Connecting to target via SWD
ConfigTargetSettings() start
Flash breakpoints are disabled.
ConfigTargetSettings() end - Took 362us
InitTarget() start
  CFG-AP DEVICEID: 0x1BB8402F
    PG2.0 device detected
  CFG-AP DEVICESTATUS: 0x034D8105
  Checking if AHB-AP is enabled...
    AHB-AP enabled --> Attaching to the target...
InitTarget() end - Took 8.05ms
Found SW-DP with ID 0x6BA02477
DPIDR: 0x6BA02477
CoreSight SoC-400 or earlier
AP map detection skipped. Manually configured AP map found.
AP[0]: AHB-AP (IDR: Not set, ADDR: 0x00000000)
AP[0]: Core found
AP[0]: AHB-AP ROM base: 0xE00FF000
CPUID register: 0x410CC601. Implementer code: 0x41 (ARM)
Found Cortex-M0 r0p1, Little endian.
FPUnit: 4 code (BP) slots and 0 literal slots
CoreSight components:
ROMTbl[0] @ E00FF000
[0][0]: E000E000 CID B105E00D PID 000BB008 SCS
[0][2]: E0002000 CID B105E00D PID 000BB00B FPB
Memory zones:
  Zone: "Default" Description: Default access mode
Cortex-M0 identified.
J-Link>erase
No address range specified, 'Erase Chip' will be executed
'erase': Performing implicit reset & halt of MCU.
ResetTarget() start
  Executing reset via SEC-AP in order to enter SACI mode...
    O.K.
  Executing exit SACI mode sequence...
    O.K.
  Checking if AHB-AP is enabled...
    O.K.
  Checking if debug probe loop entered...
    O.K.
  Invalid application entry addr detected: 0xFFFFFFFF
ResetTarget() end - Took 118ms
Device specific reset executed.
Erasing device...

****** Error: Failed to erase sectors 0 @ address 0x00000000 (Unspecified error #1)
FLASH_RAMLESS: Failed to erase target via J-Link
J-Link: Flash download: Total time needed: 0.361s (Prepare: 0.007s, Compare: 0.000s, Erase: 0.352s, Program: 0.000s, Verify: 0.000s, Restore: 0.001s)
ERROR: Erase returned with error code -5.
J-Link>exit
OnDisconnectTarget() start
  Executing SWD => dormant switching sequence...
OnDisconnectTarget() end - Took 208ms

:020000044E02AA
:20000000FFFFFFFF00000000FFFFFFFF1CDF4421FFFFFFFFFFFFFFFFAAAAAAAA00000000E8
:20002000FFFFFFFFFFFFFFFFFFFFFFFFFFFFFFFF00000000000000000000000000000000D0
:200040000000000000000000000000000000000000000000000000000000000000000000A0
:20006000000000000000000000000000000000000000000000000000000000000000000080
:20008000000000000000000000000000000000000000000000000000000000000000000060
:2000A000000000000000000000000000000000000000000000000000000000000000000040
:2000C000000000000000000000000000000000000000000000000000000000000000000020
:2000E000000000000000000000000000000000000000000000000000000000000000000000
:200100000000000000000000000000000000000000000000000000000000000000000000DF
:200120000000000000000000000000000000000000000000000000000000000000000000BF
:2001400000000000000000000000000000000000000000000000000000000000000000009F
:2001600000000000000000000000000000000000000000000000000000000000000000007F
:2001800000000000000000000000000000000000000000000000000000000000000000005F
:2001A00000000000000000000000000000000000000000000000000000000000000000003F
:2001C00000000000000000000000000000000000000000000000000000000000000000001F
:2001E0000000000000000000000000000000000000000000000000000000000000000000FF
:200200000000000000000000000000000000000000000000000000000000000000000000DE
:200220000000000000000000000000000000000000000000000000000000000000000000BE
:2002400000000000000000000000000000000000000000000000000000000000000000009E
:2002600000000000000000000000000000000000000000000000000000000000000000007E
:2002800000000000000000000000000000000000000000000000000000000000000000005E
:2002A00000000000000000000000000000000000000000000000000000000000000000003E
:2002C00000000000000000000000000000000000000000000000000000000000000000001E
:2002E0000000000000000000000000000000000000000000000000000000000000000000FE
:200300000000000000000000000000000000000000000000000000000000000000000000DD
:200320000000000000000000000000000000000000000000000000000000000000000000BD
:2003400000000000000000000000000000000000000000000000000000000000000000009D
:2003600000000000000000000000000000000000000000000000000000000000000000007D
:2003800000000000000000000000000000000000000000000000000000000000000000005D
:2003A00000000000000000000000000000000000000000000000000000000000000000003D
:2003C00000000000000000000000000000000000000000000000000000000000000000001D
:2003E0000000000000000000000000000000000000000000000000000000000000000000FD
:200400000000000000000000000000000000000000000000000000000000000000000000DC
:200420000000000000000000000000000000000000000000000000000000000000000000BC
:2004400000000000000000000000000000000000000000000000000000000000000000009C
:2004600000000000000000000000000000000000000000000000000000000000000000007C
:2004800000000000000000000000000000000000000000000000000000000000000000005C
:2004A00000000000000000000000000000000000000000000000000000000000000000003C
:2004C00000000000000000000000000000000000000000000000000000000000000000001C
:2004E0000000000000000000000000000000000000000000000000000000000000000000FC
:200500000000000000000000000000000000000000000000000000000000000000000000DB
:200520000000000000000000000000000000000000000000000000000000000000000000BB
:2005400000000000000000000000000000000000000000000000000000000000000000009B
:2005600000000000000000000000000000000000000000000000000000000000000000007B
:2005800000000000000000000000000000000000000000000000000000000000000000005B
:2005A00000000000000000000000000000000000000000000000000000000000000000003B
:2005C00000000000000000000000000000000000000000000000000000000000000000001B
:2005E0000000000000000000000000000000000000000000000000000000000000000000FB
:200600000000000000000000000000000000000000000000000000000000000000000000DA
:200620000000000000000000000000000000000000000000000000000000000000000000BA
:2006400000000000000000000000000000000000000000000000000000000000000000009A
:2006600000000000000000000000000000000000000000000000000000000000000000007A
:2006800000000000000000000000000000000000000000000000000000000000000000005A
:2006A00000000000000000000000000000000000000000000000000000000000000000003A
:2006C00000000000000000000000000000000000000000000000000000000000000000001A
:2006E0000000000000000000000000000000000000000000000000000000000000000000FA
:200700000000000000000000000000000000000000000000000000000000000000000000D9
:200720000000000000000000000000000000000000000000000000000000000000000000B9
:20074000000000000000000000000000AC54537D00000000000000000000000000000000C9
:20076000000000000000000000000000000000000000000000000000000000000000000079
:20078000000000000000000000000000000000000000000000000000000000000000000059
:2007A000000000000000000000000000000000000000000000000000000000000000000039
:2007C0000000000000000000000000000C0ED7155AA500000101020305080D156DD7E43680
:2007E000EBF431DF95AE15EE03BA8EE4C4C63FD8453F675E74D7C2012C9058E5A2947252AA
:0108000000F7
:00000001FF