Tool/software:
Hi Team,
In what conditions CC2642 chip goes to Dead condition. Unable to advisement MAC address & no functionality.
Reagrds,
Rajani
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hi Team,
In what conditions CC2642 chip goes to Dead condition. Unable to advisement MAC address & no functionality.
Reagrds,
Rajani
Hello Rajani,
Thank you for reaching out! This is a bit of an open question, could you answer these questions:
Are you running a default example from the SDK? If so, what modifications have been made to the initial example?
What SDK version are you using?
When is the device hanging and not functioning properly?
Best Regards,
Tarek
Hi Tarek,
Sorry for late reply.
problem is not resolved.
SDK we are using 'Simplelink_cc13x2_26x2_sdk_5_20_00_52\examples\rtos\CC26X2R1_LAUNCHXL\ble5stack'
We are running our own application.
The FW is working well.
The problem we are observing intermediate not always. 20times Flashing FW via JTAG 5 times found this issue. Unable to get BT MAC address, unable to communicate to CC2642 chip. Tried SW RESET, not working
Not sure device went unknown stat or Dead or FW is not there.
Same HW is working next time FW erase, loading.
Suggest options to identify root cause.
Thanks,
Rajani
Hello Rajani,
I'm sorry for to hear that! What example from the SDK are you using? Also, are you attempting to change the MAC Address (also known as the BLE address)? And have you tried debugging this issue? If not, could you try and let me know when the device goes into the "dead" state you've described?
Best Regards,
Tarek
Hi Tarek,
Production script we are writing MAC address. Like 0017557977BF
We started debugging this issue put some buzzer indication at different location in code. But when problem observed the code is not hitting Buzzer.
We are using Elprotronic Gang Pro CC Flash programming tool is using. Is any issue
SDK we are using BLE multirole peripheral/central.
Regards,
Rajani
Hello Rajani,
Thank you for providing this information! I do have a few more questions regarding this matter:\
Best Regards,
Tarek
Hi Tarek,
1. Attached Pitcher
2.We are using Elprotronic-GangPro ARM. Attached config file below. Please help me if anything we are missing.
3. Different MAC Address are written
Regards,
Rajani
;============= FlashProCMx configuration =============
MCU_name CC2642R1F
Target_EN 51
EnableBlankCheck 1
FlashEraseModeIndex 2
WriteLockingBitsEn 1
NotEraseSegmentIfBlank 1
VerifyProtection 1
ForceEraseEEPROM 0
EraseMemIfLockedEn 0
AlwaysUseFactoryEraseEn 0
Interface 10
ResetTimeIndex 0
ResetPulseTime 10
ResetIdleTime 10
ResetVccOffTime 50
Reset_3st_mode_en 1
NTRST_en 1
ApplProgramRunTime 0
VccFromFPAin_mV 3300
PowerFromFpaEn 1
ReleaseJtagState 0
RetainDefinedData 0
FlashReadModeIndex 1
VerifyModeIndex 2
VccSettleTime 100
WrIncludingLockedSegm 0
RdIncludingLockedSegm 0
EraseDefMainMemEn 0
DefOTPWriteEnable 0
DefEFWriteEnable 0
ReadDefMainMemEn 0
ReadDefInfoMemEn 0
ReadDefEFMemEn 0
SerializationEnable 0
SNDispFormatIndex 0
SNMemFormatIndex 1
ModelTextEnable 0
ModelTextSize 2
ModelDataType 0
SNInfoMode 0
SNExistWarnEn 1
RemoveCodefromSNlocationEn 0
Custom_SN_size 4
BarCodeReaderEnable 0
BarCodeAutoStartEnable 0
PostAmbleIndex 0
GUIDisplayFormat 0
ApplicationStartEnable 1
CodeFileReload 0
CC_MemoryProtSource 0
CC_USER_DBG_WrEn 0
CC_26xx_MemoryProtSource 0
CC_26xx_GenOpt_WrEn 1
CC_26xx_Prot_WrEn 0
CC_26xx_USER_DBG_WrEn 1
BeepOkEnable 1
PCSpeaker 1
OverwriteEmptyValues 0
DisplayErrorOnce 0
PromptForPowerCycle 1
PowerCycleDelay 100
PromptForFirstPageErase_coreM0only 1
DispSkipBlankLines 1
JTAG_Chain_Enable 0
JTAG_Chain_IR_header_delay 0
JTAG_Chain_DR_header_delay 0
JTAG_Chain_IR_tail_delay 0
JTAG_Chain_DR_tail_delay 0
JtagIRsizeDevice-1 0
JtagIRsizeDevice-2 0
JtagIRsizeDevice-3 0
JtagTAPsDevice-1 0
JtagTAPsDevice-2 0
JtagTAPsDevice-3 0
JtagSelDevice-1 0
JtagSelDevice-2 0
JtagSelDevice-3 0
CS1_Enable 0
CS2_Enable 0
CS3_Enable 0
CS4_Enable 0
CS_type_index 0
CS_Init_index 0
CS_Result_index 0
CS_code_overwrite_en 0
Graph_MeasureMode_index 7
Graph_SamplingRate_index 3
Graph_MeasureCurrent_index 0
Graph_Ratio1 25
Graph_Ratio2 75
Graph_Scale2 1
Graph_InvAlpha 10
DefEraseFlashStart 0x0000
DefEraseFlashStop 0xDFFFFFFF
DefOTPWriteStart 0x0000
DefOTPWriteStop 0x0000
DefEraseEFStart 0x0000
DefEraseEFStop 0x0000
DefReadStartAddr 0x0000
DefReadStopAddr 0xDFFFFFFF
DefOTPStartAddr 0x0000
DefOTPStopAddr 0x0000
DefReadEFStart 0x0000
DefReadEFStop 0x0000
RetainDataStart 0x0000
RetainDataStop 0x0003
SNStartAddress 0x0000
ModelTextStartAddr 0x0000
Starting_SN 0x0000
Ending_SN 0x0000
SN_increment 0x0001
JTAG-Clk-frequency 0x1388
CLK_frequency 0x4E20
CC-LOCKPAGE0-Data 0x0000
CC-LOCKPAGE1-Data 0x0000
CC-LOCKPAGE2-Data 0x0000
CC-LOCKPAGE3-Data 0x0000
CC-LOCKPAGE4-Data 0x0000
CC-LOCKPAGE5-Data 0x0000
CC-LOCKPAGE6-Data 0x0000
CC-LOCKPAGE7-Data 0x0000
CC-26xx-CCFG-31-0 0xFFFFFFFF
CC-26xx-CCFG-63-32 0xFFFFFFFF
CC-26xx-CCFG-95-64 0xFFFFFFFF
CC-26xx-CCFG-127-96 0xFFFFFFFF
CC-26xx-CCFG-BL-CONFIG 0xFFFFFF
CC-26xx-CCFG-ERASE-CONF 0x0000
CC-26xx-CCFG-IMAGE-VALID 0x0000
CC-26xx-CCFG-TI-BACKDOOR 0xFFFFFF00
CC-26xx-CCFG-TAP-DAP0 0xFF000000
CC-26xx-CCFG-TAP-DAP1 0xFF000000
CS_Polynominal 0x0000
CS1_StartAddress 0x0000
CS1_EndAddress 0x0000
CS1_ResultAddress 0x0000
CS2_StartAddress 0x0000
CS2_EndAddress 0x0000
CS2_ResultAddress 0x0000
CS3_StartAddress 0x0000
CS3_EndAddress 0x0000
CS3_ResultAddress 0x0000
CS4_StartAddress 0x0000
CS4_EndAddress 0x0000
CS4_ResultAddress 0x0000
SNFilePathAndName
ModelCode 00 00
Hello,
I understand you are using the Elprotronic-GangPro ARM, but just as a test, could you attempt to use the XDS110 and let me know if that works
Best Regards,
Tarek