Other Parts Discussed in Thread: CC2652R7,
Tool/software:
Hi Team,
I am currently trying to add the OAD on-chip feature to my firmware on CC2652R7. I try to use BTool to send a new image to do the OAD, but it failed as the picture shows:
I am using simplelink_cc13xx_cc26xx_sdk_7_40_00_77 and CCS 12.8.1, and first flashed these files as Simplelink Academy suggest:
Why the log in BTool shows
[3877] : <Info> - 12:45:36.023
OAD ImageControl Response
Command ID = 0x12 (ImageBlockWriteRsp)
Status = 0x09 (OAD_INCOMPATIBLE_IMAGE)
Is this the reason OAD download failed? Or anything else I can check? I have learned and follow the Simplelink Academy Bluetooth Low Energy Enhanced Over the Air Download (OAD) Fundamentals
and Bluetooth Low Energy Enhanced Over the Air Download (OAD) Advanced, but still failed to use the on-chip OAD feature.
Could anyone help with that, thanks a lot!!!
Best regards,
Jermyn