Part Number: CC2340R5
Other Parts Discussed in Thread: UNIFLASH
Tool/software:
Hi
I've got a custom design with a CC2340R5 SOC, that I have worked for a while using CCS and UNIFLASH connected via the SWD part of a CC3220 Lauchpad I had laying around. I have used CCS version 12.3.0.00005 and UNIFLASH version 9.1.0.5175 (and also version 8.5.0 earlier). I had never had an issue programming or debugging it.
Now the design has made it to production, the production house is unable to program these devices with an XDS110. They get the error:
[ERROR] Cortex_M0P: File Loader: Memory write failed: Target did not enter SACI after pin reset
I have now tested this here and I get the same error when using my own XDS110.
I have used the same XDS110 for a bunch of other processors, CC26xx and for those it works fine.
I just wanted to find out if there is a way to solve this via software before I post them one of my launchpad's in order to program as this is quite urgent now, it's holding up production.
Thanks
Reto