Part Number: CC2745R10-Q1
Tool/software:
I have executed the following sample program from the SDK, but it stops at Exception_handlerSpin at ExceptionArmV8M.c
Specifically, it seems that an error is occurring in vListInsert() within list.c.
Could you please provide any solutions or workarounds for this issue?
This code is a combination of the sample code from CryptoKeyKeyStore_PSA and empty.c
SDK version is 8.40.02.01
#include <unistd.h>
#include <stdint.h>
#include <stddef.h>
/* Driver Header files */
#include <ti/drivers/GPIO.h>
// #include <ti/drivers/I2C.h>
// #include <ti/drivers/SPI.h>
// #include <ti/drivers/Watchdog.h>
#include <ti/drivers/cryptoutils/cryptokey/CryptoKeyKeyStore_PSA.h>
#include <ti/drivers/cryptoutils/cryptokey/CryptoKeyKeyStore_PSA_helpers.h>
/* Driver configuration */
#include "ti_drivers_config.h"
/*
* ======== mainThread ========
*/
void *mainThread(void *arg0)
{
uint8_t keyingMaterial[16] = {0x1f, 0x8e, 0x49, 0x73, 0x95, 0x3f, 0x3f, 0xb0,
0xbd, 0x6b, 0x16, 0x66, 0x2e, 0x9a, 0x3c, 0x17};
CryptoKey cryptoKey;
KeyStore_PSA_KeyFileId keyID;
int_fast16_t status;
KeyStore_PSA_KeyAttributes attributes = KEYSTORE_PSA_KEY_ATTRIBUTES_INIT;
// Assign key attributes
KeyStore_PSA_setKeyUsageFlags(&attributes, (KEYSTORE_PSA_KEY_USAGE_DECRYPT | KEYSTORE_PSA_KEY_USAGE_ENCRYPT));
KeyStore_PSA_setKeyAlgorithm(&attributes, KEYSTORE_PSA_ALG_CCM);
KeyStore_PSA_setKeyType(&attributes, KEYSTORE_PSA_KEY_TYPE_AES);
KeyStore_PSA_setKeyLifetime(&attributes, KEYSTORE_PSA_KEY_LIFETIME_PERSISTENT);
// Set key ID
GET_KEY_ID(keyID, KEYSTORE_PSA_KEY_ID_USER_MIN);
KeyStore_PSA_setKeyId(&attributes, keyID);
// Import the keyingMaterial
status = KeyStore_PSA_importKey(&attributes, keyingMaterial, sizeof(keyingMaterial), &keyID);
if (status != KEYSTORE_PSA_STATUS_SUCCESS)
{
// Handle error
}
// Initialize cryptoKey for crypto operations
KeyStore_PSA_initKey(&cryptoKey, keyID, sizeof(keyingMaterial), NULL);
// Use the cryptoKey for AESCCM operations
// Destroy key after use
status = KeyStore_PSA_destroyKey(keyID);
if (status != KEYSTORE_PSA_STATUS_SUCCESS)
{
// Handle error
}
while (1)
{
}
}
Best regards,