Tool/software:
Hi all
We are using a DIO pin configured as an input with no internal pull-up or pull-down resistor, and an external 1MΩ pull-up resistor connected.
The pull-up voltage is 2.7V, but the voltage measured at the DIO pin is 2.27V.
How many leak current in DIO pin with no internal pull-up or down resistor?
And is this voltage drop considered normal behavior due to the input leakage current?