This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2340R5-Q1: About I2C Driver for Controller and Target

Part Number: CC2340R5-Q1
Other Parts Discussed in Thread: CC2340R5

Tool/software:

Hi, TI Team.

Please provide information on the operation of both the I2C controller and the target regarding the following:

Q1) Is the level operation of SCL and SDA necessary for bus communication, including ACK/NACK checking and the generation of start/stop conditions in I2C communication, controlled by hardware or software?

Q2) Does it support clock stretching functionality?

Q3) What happens when there is a timing conflict with the BLE task?

Best Regards.

  • Hello,

    Here is the documentation for the I2C driver: I2C.h File Reference & I2CLPF3.h File Reference more device specific restrictions. I2CTarget.h File Reference contains information regarding target I2C.

    Additionally, detailed information can be found in the TRM Chapter 21 Inter-Integrated Circuit (I2C). This has a lot of information regarding the I2C peripheral, especially if you choose not to use our I2C driver.

    Q1) Is the level operation of SCL and SDA necessary for bus communication, including ACK/NACK checking and the generation of start/stop conditions in I2C communication, controlled by hardware or software?

    The driver should handle this for. However, please pay close attention to the difference between the controller and target drivers. I have linked both above.

    Q2) Does it support clock stretching functionality?

    Yes.

    Q3) What happens when there is a timing conflict with the BLE task?

    It is up to the developer to handle this case. It should be noted that the BLE task should have the highest priority.

    Best,

    Nima Behmanesh

  • Hi, Nma.

    Thank you for your prompt response.

    Could you please explain a bit more specifically? Let me rephrase my question.

    Q1)We are assuming the use of a driver, so please provide information only for cases where the driver is used.

    When using the driver, operations such as start/stop are executed within the API, so is it correct to understand that users can use it without having to interrupt any operations?

    Also, since the actions are performed within the API, is it correct to understand that the CC2340R5 is executing these processes through software?

    Q2)Thanks.

    I believe the content you are addressing pertains to cases where the CC2340R5 is receiving. When the CC2340R5 is transmitting, can the clock-stretching function be used if the transmission data is not ready or if other high-priority processes are being executed?

    Is there anything the user needs to do in such situations?

    Q3)Please tell me about the operations within the driver.

    Since it's confirmed in Q2 that the clock-stretching function can be used, can the driver autonomously use this function to pause I2C communication when a higher priority process conflicts, and then resume I2C communication once the priority process is completed?

    I'm sorry for the lengthy message, but I appreciate your cooperation.

    Best Regards.

  • Hello,

    I apologize, but I'm a bit confused on what you're asking.

    When using the driver, operations such as start/stop are executed within the API, so is it correct to understand that users can use it without having to interrupt any operations?

    Yes, the operations such as start/stop are executed within the API, but not sure what you mean by using it without having to interrupt operations. In the documentation I provided before (https://dev.ti.com/tirex/content/simplelink_lowpower_f3_sdk_8_40_00_61/docs/drivers/doxygen/html/_i2_c_8h.html) there two I2C modes that may be used: blocking and callback. For blocking, the I2C_transfer function will not return until it's done. In callback, the transactions are queued. I recommend reading this section for more information.

    Additionally, please refer to the I2C source code in the SDK. All of the drivers have their source code availabe in the SDK. You can refer to <sdk>/source/ti/drivers/i2c

    I believe the content you are addressing pertains to cases where the CC2340R5 is receiving. When the CC2340R5 is transmitting, can the clock-stretching function be used if the transmission data is not ready or if other high-priority processes are being executed?

    Is there anything the user needs to do in such situations?

    Are you referring to the Target or Controller? The Controller should handle all of that for you. The Target however, the developer will need to implement. There is a portion of the TRM that implies the target may stretch the clock:

    I've contacted a colleague for more information regarding this.

    Q3)Please tell me about the operations within the driver.

    Since it's confirmed in Q2 that the clock-stretching function can be used, can the driver autonomously use this function to pause I2C communication when a higher priority process conflicts, and then resume I2C communication once the priority process is completed?

    Please refer to the driver source code and the driver information.

    Best,

    Nima Behmanesh

  • Hi, Nma.

    Thanks for the reply.

    Q1)

    Regarding Q1, I apologize for the confusion.

    To put it simply, for the controller, you just need to perform the I2C_transfer() from the API reference.

    For the target, I wanted to reconfirm that by merely executing I2CTarget_start() and manipulating data within the callback function: targetCallbackFxn(), as described in the example, I2C communication can be performed without issues.

    I wish to confirm that necessary voltage operations on the I2C bus, such as start, stop, and ACK, do not require the user to manipulate registers, etc. Additionally, I would like to know whether these operations are performed by the device via hardware or software.

    Q2)

    Regarding Q2, it's the same; I want to confirm whether the clock-stretching function can be used during read/write operations regardless of whether it's the controller or target.

    Also, I'd like to know if any special operations beyond executing the API, such as setting registers by the user, are necessary.

    Q3)

    I will close Q3.

    I apologize for asking repeatedly, but I appreciate your cooperation.

    Best Regards.

  • Hello,

    For the target, I wanted to reconfirm that by merely executing I2CTarget_start() and manipulating data within the callback function: targetCallbackFxn(), as described in the example, I2C communication can be performed without issues.

    I wish to confirm that necessary voltage operations on the I2C bus, such as start, stop, and ACK, do not require the user to manipulate registers, etc. Additionally, I would like to know whether these operations are performed by the device via hardware or software.

    You should treat the callback function as an interrupt. No major processing should occur in the callback. I recommend storing the data somewhere, and enqueuing an event in the callback so that the application can do the processing.

    As far as voltage operations, you will need a level shifter. For instance, the CC2340R5 runs on 3.3v so if the target device is at a lower voltage, a level shifter will be needed. As far as start, stop, ack, etc. the driver will handle this. The only thing you will need to set is the voltage levels via an external level shifter.

    Q2)

    Regarding Q2, it's the same; I want to confirm whether the clock-stretching function can be used during read/write operations regardless of whether it's the controller or target.

    Also, I'd like to know if any special operations beyond executing the API, such as setting registers by the user, are necessary.

    After speaking with the team, the target configuration does support clock stretching, but the controller does not. The target code will handle the clock stretching for you.

    I apologize for asking repeatedly, but I appreciate your cooperation.

    No worries at all! Thank you for your clarifications and patience!

    Best,

    Nima Behmanesh

  • Hello, Nima.

    I understand completely, thank you.

    Let me confirm just two more points:

    Q4) In the case of the controller, there's no clock-stretching function.

    In other words, if the counterpart (target) of CC2340R5 tries to use SCL for clock stretching by pulling it low, will CC2340R5 forcibly continue the communication?

    Q5) If a higher priority task arises during I2C communication with CC2340R5 as the controller, does it simply pause clock output and restart clock output after resuming the task?

    Best Regards.

  • Hello,

    Q4) In the case of the controller, there's no clock-stretching function.

    In other words, if the counterpart (target) of CC2340R5 tries to use SCL for clock stretching by pulling it low, will CC2340R5 forcibly continue the communication?

    I believe so. I've asked a colleague to get more information regarding this.

    Q5) If a higher priority task arises during I2C communication with CC2340R5 as the controller, does it simply pause clock output and restart clock output after resuming the task?

    Reading through the driver code, it appears that during the transfer, interrupts are disabled. However, the driver code should be analyzed since the implementation is public.

    Best,

    Nima Behmanesh

  • Hello,

    To follow up on clock stretching, if the target and the controller are both CC2340R5, then the controller will recognize that clock stretching is occurring, and will handle it accordingly. It will properly pause the communication. 

    Best,

    Nima Behmanesh