This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC256XQFNEM: BL6450Q

Part Number: CC256XQFNEM

Tool/software:

HI TI member.

      We are working on the Bluetooth certification tests.

     we want the DUT to be in continuous transmission mode for about 10 minutes(CW and also modulated wave).

     Currently, it seems to only last for 9 seconds.

   could you please tell me the command?

 

for example:  we are using this commands in below:

   and i also tried using these commands , but it didn't be better...not any change...

     1.   HCI_VS_DRPb_Tester_Packet_TX_RX = 0x03, 0x00,  0x00,  0x05, 0x01, 0x53,  0x0F, 0x00, 0x01 ,0xFF   //Single freq, TX Channel 0, RX Channel 0 ,DH5 , PRBS, 339 , 15dBm ,enable whitening, max511 

    2.  HCI_VS_DRPb_Tester_Con_TX =  0x01, 0x00, 0x00, 0x0F, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00  // GFSK, PN9, channel 0, power=15dBm, 

so could you please check it again.  

if have any incorrect, please tell me the correct flow of the commmands thanks

B,R

HEJUN