Other Parts Discussed in Thread: CC1350
Tool/software:
-
I am working on an RF project based on the CC2340, using RF proprietary mode.
I am curious about can I connect a CC2340 with a CC2652 or CC1350 using RF proprietary,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Huy,
Not a CC1350 since this device only supports Sub-1 GHz frequency bands whereas the CC2340 and CC2652 are 2.4 GHz only devices. However it is possible to communicate between the CC2340 and CC2652 using a shared PHY such as the 250 kbps MSK PropRF or even IEEE 802.15.4. You can perform an initial analysis with SMARTRFTM-STUDIO before developing application code starting from the PropRF examples in the SimpleLink F2/F3 SDKs.
Regards,
Ryan