I have two CC2540EM. Both of them are having the same IEEE Adreess (0xC0FFEEC0FFEE). Is all cc2540 has the same address? how can i distinguish two modules with the BTLE stack? The Rev number of the modules is Rev .1.5.1.1
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I have two CC2540EM. Both of them are having the same IEEE Adreess (0xC0FFEEC0FFEE). Is all cc2540 has the same address? how can i distinguish two modules with the BTLE stack? The Rev number of the modules is Rev .1.5.1.1
Hi Leo,
Some of our early chips has that address. You can overwrite the secondary IEEE address with the TI Flash Programmer. If the secondary address differs from 0xFFFFFFFFFFFF (which is the default), then it will be used instead of the primary address.
BR