Part Number: CC2340R5
Tool/software:
Hi Expert,
LCM w/ SPI interface is proposed to use in our program.
- since the CC2340 just supports one SPI interface, we want to share the SPI interface w/ the external flash. the diagram is in below. SPI speed is better to configured more than 10MHz.

- the display resolution is 60*100, and the bit depth is 16 bits. if we use SRAM for the display buffering, it might need 24KB SRAM for the buffering(double buffering). it seems the SRAM usage is too big for our application. I'm wondering if can use uDMA feature to directly transfer display data(eg: image) from external flash to the LCD module over SPI interface.
could you please help to evaluate the possiblity of using CC2340R5 to drive LCD? Thanks.
BR,
Guangwen