This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2340R5: Compare table of TLSR8208G

Part Number: CC2340R5

Tool/software:

Hi Team, 

Can you help to provide the compare table of CC2340R52 between TLSR8208? The application is E-cig. Thanks!

  • Hi,

    I am asking some of our internal team members about this competitive analysis. I will report back in case I have any additional details. 

    Do you have a high level block diagram or design requirements for this design? This could help highlighting the most important aspects of our solution. 

    Also, do you have any information about the "G" variant of the TLSR8208? The online information I could find does not have this specific variant.

    Regards,

    Rafael

  • Hi,

    Please check the high level comparison table below between the two device families.

     

    Device

    CC2340R5

    TLSR8208(A,B,C,D)

    Core

    M0+

    32-bit Proprietary core

    Flash /

    SRAM

    Up to 512kB /

    Up to 64kB

    Up to 512kB /

    16kB  

    Power Consumption

    TX @0dbm: 5.1mA

    TX @8dbm: <11mA

    RX: 5.3mA

    Standby: <710nA (Full RAM Retention)

    TX @ 0dBm: 9.5mA

    RX: 9.1mA

    Standby: 0.9uA (16kB SRAM Retention)

    Protocols

    Bluetooth LE

    Zigbee

    Thread

    Bluetooth LE

    Zigbee

    Proprietary

     

    Peripherals

    1x UART

    1x SPI

    1x I2C

    1x UART

    1x SPI

    1x I2C

    GPIOS

    Up to 26

    Up to 38

    Temp Support

    -40C to 125C

    -40C to 85C

    Package

    QFN40(5x5)

    QFN24(4x4)

    WCSP (2.2x2.6)

    QFN(7x7) – TLSR8208A

    QFN(4x4) – TLSR8202B

    QFN(5x5) – TLSR8208C

    SOP(9.9x6) – TLSR82028D

    Hope this helps,

    Rafael