Part Number: CC2340R5
Tool/software:
Hi,
we want to enable to BLE hop test. may I know whether the command below correct? also, we are using sdk_7_20_01_10, whether hop test is supported?
[7] : <Tx> - 05:16:50.397
-Type : 0x01 (Command)
-OpCode : 0xFC28 (HCIExt_EnhancedModemHopTestTxCmd)
-Data Length : 0x03 (3) byte(s)
PayloadLength : 0x00 (0)
DtmPktPattern : 0x01 (1) (Dtm_0x0F)
SetupPhyParam : 0x00 (0) (One_Mbps_Phy)
Dump(Tx):
0000:01 28 FC 03 00 01 00