This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2640R2F-Q1: Bluetooth module recommendation

Part Number: CC2640R2F-Q1
Other Parts Discussed in Thread: CC2564C

Tool/software:

Hi TI team ,

Could you help to recommend a Bluetooth module to meet the below requirement:

  • BT version:5.3
  • Dual mode(BR/EDR+LE)
  • Support LE audio
  • AEC-Q100
  • Operating voltage :1.7V-5.5V
  • Operating temperature: -40℃ -105℃

Thanks a lot!

  • Hi,

    Unfortunately, we do not have a bluetooth chip that meets all of the above requirements. The big holdback is the dual mode support. We only have the CC2564C device that supports BR/EDR + LE but unfortunately it is only specd upto the 5.1 BT SIG spec. It also does not support LE Audio.

    Best,

    Rogelio