This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2340R5: Very high current draw after enabling internal DCDC

Part Number: CC2340R5
Other Parts Discussed in Thread: SYSCONFIG

Tool/software:

I'm using a custom PCB. Here's the CC2340R5 portion of the schematic:

When I enable the internal DCDC the idle current draw with no radio activity is 50mA at 3V! If I change the voltage regulator in sysconfig from DCDC to the GLDO, the current draw is ~0mA at 3V (I'm using a power supply that can't measure under 1mA).

I was under the impression that the DCDC is more efficient than the GLDO?