Tool/software:
Hello;
In fact we have been testing the channel sounding SDK, we want to use the PBR+RTT but we found that in this sdk only PBR is developped.
1. The question can we add the RTT methods based on this SDK does it has all necessary features. the sdk support the RTT if developped.
2. When we change the ACI upper that 1, we run the distance measure.py file it gives always ACI=0 and the distance, confidence and quality has a fixed random measurement.
3. When upgrading the number of the car-node antenna, it is described that we have to enable PBEGPO2 and PBEGPO3.
4. For those pin it is written that those pin are
So the question, do we need the antenna booster pack to upgrade the number of antenna. If yes, how can we get it.
5. Another question is related to the handover example, when trying to use two key_nodes with one car_node it always gives an error of not knowing the nodes.
is there a more detailed description on how to test it.
Thank you;
Best Regards;