Hi All,
Any ideas on how to load a text file to Slave or Master CC2540 Module then wirelessly transfer the text file data to Master or Slave CC2540 Module?
Regards,
Daniel L
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi All,
Any ideas on how to load a text file to Slave or Master CC2540 Module then wirelessly transfer the text file data to Master or Slave CC2540 Module?
Regards,
Daniel L
Hi Dan,
Please read:
http://e2e.ti.com/support/low_power_rf/f/538/p/108807/384844.aspx
And this:
http://e2e.ti.com/support/low_power_rf/f/538/t/123119.aspx
There is a maximum buffer for notifications.
They are short threads with important info about what you are requiring ;) Good luck!
Hi Kazola,
Many thanks for your links. They help.
In addition, do you know or know who knows about how to load and send data wirelessly by coding in C language? I'm not sure how to write C applications to do that.
Regards,
Hi Daniel,
sorry for the delay in answering. Verify this post since you have asked the same thing in another thread ;) I've detected you. I'll help you in the other place but perhaps IAR is not the most convenient plattform for a beginner....
Thanks!
Hi Kazola,
That's OK! I'm also working myself to see how to move forward. Let me know if you have some ideas.
I intend to send the following text file wirelessly using C language.
// Start Time: 0 // Sample rate: 100.0Hz // Scenario: 5.9 // Firmware Version: 2.6.1 Counter Temperature Acc_X Acc_Y Acc_Z Gyr_X Gyr_Y Gyr_Z Mag_X Mag_Y Mag_Z Roll Pitch Yaw AnalogIn_1 AnalogIn_2 31436 0.00 -0.333117 9.467282 -2.555237 -0.005013 -0.026711 -0.008481 0.046978 0.628360 -0.648472 105.145493 2.010289 -80.986580 0 0 31437 0.00 -0.310348 9.482548 -2.562759 -0.006816 -0.028514 -0.004904 0.049285 0.630327 -0.651331 105.142212 2.015929 -80.999229 0 0 31438 0.00 -0.310250 9.475011 -2.555179 -0.011358 -0.023141 -0.004849 0.048844 0.628924 -0.647185 105.135963 2.020574 -81.006882 0 0 31439 0.00 -0.340742 9.467246 -2.524627 -0.010497 -0.018652 0.002284 0.049287 0.629607 -0.651048 105.130722 2.020746 -81.015152 0 0 31440 0.00 -0.356048 9.467123 -2.524619 -0.010632 -0.001563 0.005897 0.048984 0.630502 -0.648180 105.125252 2.016219 -81.014313 0 0 31441 0.00 -0.402404 9.504479 -2.508935 -0.010695 0.003822 0.013047 0.048576 0.627881 -0.651340 105.120270 2.007090 -81.011749 0 0 31442 0.00 -0.432581 9.466498 -2.532227 0.000422 -0.030307 -0.005865 0.046252 0.629381 -0.648323 105.120636 2.013366 -81.027550 0 0 31443 0.00 -0.432056 9.421222 -2.555607 -0.007659 -0.030341 -0.013816 0.048567 0.629616 -0.651047 105.116882 2.024249 -81.039886 0 0 31444 0.00 -0.432392 9.451419 -2.524718 -0.033818 -0.030480 -0.001102 0.046671 0.630835 -0.646457 105.097595 2.027912 -81.053177 0 0 31445 0.00 -0.416878 9.436482 -2.494263 -0.013810 -0.051974 -0.008474 0.046837 0.629640 -0.650900 105.089859 2.039099 -81.078300 0 0 31446 0.00 -0.371339 9.467011 -2.509308 -0.002956 -0.065408 0.012782 0.047109 0.630245 -0.647319 105.087494 2.040287 -81.113159 0 0 31447 0.00 -0.333097 9.467301 -2.532283 -0.019208 -0.059177 0.004034 0.046831 0.630082 -0.649896 105.076439 2.045620 -81.144127 0 0 31448 0.00 -0.294686 9.452493 -2.570703 -0.015757 -0.042955 0.017414 0.045960 0.629108 -0.646892 105.067154 2.040890 -81.168686 0 0 31449 0.00 -0.332781 9.437085 -2.586126 -0.004985 -0.033906 0.005756 0.046547 0.629647 -0.650470 105.064743 2.041476 -81.185928 0 0 31450 0.00 -0.332781 9.437085 -2.586126 -0.019395 -0.033977 0.003212 0.045085 0.630571 -0.646025 105.053627 2.043262 -81.203079 0 0 31451 0.00 -0.355718 9.436919 -2.563159 -0.003440 -0.001522 0.014743 0.046258 0.629654 -0.650183 105.052689 2.034050 -81.203728 0 0 31452 0.00 -0.424585 9.436370 -2.555469 -0.010490 -0.019563 0.005846 0.046525 0.631127 -0.646312 105.046944 2.032230 -81.211784 0 0 31453 0.00 -0.416723 9.421371 -2.525011 -0.007743 -0.023151 0.002244 0.046972 0.630514 -0.649751 105.043182 2.033190 -81.222549 0 0 31454 0.00 -0.416619 9.413840 -2.509779 -0.017492 -0.042995 -0.001288 0.046389 0.629968 -0.647032 105.033005 2.038800 -81.243668 0 0 31455 0.00 -0.370976 9.436840 -2.509592 -0.024703 -0.044822 0.002338 0.046107 0.630242 -0.649178 105.019096 2.042945 -81.266449 0 0 31456 0.00 -0.355550 9.421821 -2.578604 -0.010357 -0.037538 0.005793 0.044653 0.631146 -0.646881 105.013077 2.043818 -81.286713 0 0 31457 0.00 -0.309655 9.422173 -2.601584 -0.006863 -0.023112 0.004019 0.045814 0.630828 -0.648603 105.009811 2.043796 -81.297722 0 0 31458 0.00 -0.324828 9.414544 -2.555739 0.007553 -0.019452 -0.004125 0.044360 0.631591 -0.646020 105.014465 2.047472 -81.305374 0 0 31459 0.00 -0.370640 9.406643 -2.540481 -0.006842 -0.023135 0.002234 0.044668 0.630254 -0.649891 105.011215 2.048440 -81.316132 0 0 31460 0.00 -0.393611 9.406445 -2.555771 0.011207 -0.026645 0.000280 0.045515 0.631285 -0.646310 105.017792 2.050746 -81.327301 0 0 31461 0.00 -0.386022 9.414075 -2.525099 0.014923 -0.039225 -0.006919 0.045820 0.629815 -0.648893 105.026741 2.059190 -81.345612 0 0 31462 0.00 -0.332390 9.406940 -2.555805 0.010494 -0.050026 -0.006909 0.043649 0.630434 -0.647312 105.032478 2.068952 -81.371033 0 0 31463 0.00 -0.301857 9.414742 -2.540449 0.007661 -0.033845 -0.003275 0.045099 0.629968 -0.648891 105.037354 2.074562 -81.386902 0 0 31464 0.00 -0.240949 9.437826 -2.586178 0.009292 -0.015824 0.005674 0.043933 0.631584 -0.647451 105.043015 2.072280 -81.393532 0 0 31465 0.00 -0.248700 9.445301 -2.593754 0.007350 0.000358 0.012867 0.045674 0.630534 -0.649463 105.048294 2.063811 -81.392853 0 0 31466 0.00 -0.279381 9.452617 -2.570712 0.002896 -0.000569 -0.006701 0.043932 0.631158 -0.646594 105.050667 2.066109 -81.389709 0 0 31467 0.00 -0.340497 9.444592 -2.555446 0.003640 0.018310 0.004039 0.044821 0.629377 -0.650897 105.054222 2.059826 -81.377777 0 0 31468 0.00 -0.401459 9.421456 -2.570927 0.009114 0.005729 0.019996 0.044935 0.631444 -0.645449 105.060135 2.046414 -81.374405 0 0 31469 0.00 -0.432197 9.436346 -2.509557 0.003851 -0.010507 0.012870 0.046398 0.628946 -0.648325 105.063202 2.039570 -81.379745 0 0 31470 0.00 -0.355348 9.406754 -2.555793 0.007465 -0.010464 0.007487 0.044946 0.629848 -0.646315 105.067917 2.035491 -81.384392 0 0 31471 0.00 -0.340433 9.437024 -2.586122 0.025401 -0.001369 0.007353 0.044674 0.629242 -0.650039 105.083534 2.030338 -81.383858 0 0 31472 0.00 -0.309591 9.414604 -2.632260 0.018180 0.002210 0.000297 0.045234 0.629558 -0.646030 105.094681 2.028347 -81.379982 0 0 31473 0.00 -0.301834 9.407135 -2.617033 0.010978 0.002173 -0.000530 0.045248 0.629240 -0.649467 105.102142 2.027006 -81.376312 0 0 31474 0.00 -0.340161 9.414395 -2.586335 0.009210 -0.001448 -0.001415 0.044658 0.630564 -0.647456 105.108086 2.026508 -81.375038 0 0 31475 0.00 -0.355829 9.444443 -2.586042 0.009182 0.002149 -0.004966 0.046398 0.629518 -0.648895 105.114548 2.027624 -81.370712 0 0 31476 0.00 -0.386719 9.466819 -2.593463 0.001863 0.012902 0.005827 0.043800 0.629275 -0.647460 105.116524 2.020975 -81.362938 0 0 31477 0.00 -0.401836 9.451615 -2.585945 0.007537 -0.022161 0.006569 0.046402 0.630365 -0.651183 105.121513 2.019370 -81.373795 0 0 31478 0.00 -0.371030 9.436790 -2.570802 0.018406 -0.026601 -0.001565 0.044670 0.628967 -0.648465 105.132225 2.022714 -81.385025 0 0 31479 0.00 -0.309796 9.437296 -2.555534 0.011150 -0.024833 0.014545 0.045694 0.628062 -0.651477 105.139191 2.017096 -81.398560 0 0 31480 0.00 -0.294490 9.437420 -2.555543 0.006651 -0.019449 -0.007680 0.044670 0.628967 -0.648465 105.143349 2.022755 -81.405540 0 0 31481 0.00 -0.263914 9.437635 -2.593817 0.005631 -0.006848 0.000386 0.045538 0.629660 -0.650468 105.147568 2.022237 -81.406990 0 0 31482 0.00 -0.279394 9.452603 -2.586015 -0.000825 0.011108 0.005842 0.045247 0.628387 -0.647896 105.147964 2.015844 -81.398834 0 0 31483 0.00 -0.302547 9.467491 -2.601162 -0.010818 0.023654 -0.002942 0.045108 0.629519 -0.650754 105.143364 2.012568 -81.382904 0 0 31484 0.00 -0.325351 9.452195 -2.631896 0.000052 0.016513 -0.004842 0.045673 0.629251 -0.647464 105.144424 2.011275 -81.370338 0 0 31485 0.00 -0.371434 9.466923 -2.616426 -0.005399 0.020071 0.004131 0.045396 0.628944 -0.650041 105.142822 2.004628 -81.357452 0 0 31486 0.00 -0.416805 9.421295 -2.616826 -0.007130 0.010155 0.013028 0.045381 0.628979 -0.646033 105.139549 1.994405 -81.351738 0 0 31487 0.00 -0.454886 9.405900 -2.616947 -0.017888 0.007398 0.000640 0.046539 0.630094 -0.648893 105.130577 1.991644 -81.345345 0 0 31488 0.00 -0.401318 9.406333 -2.616977 0.001999 -0.005091 0.012901 0.045092 0.629413 -0.646317 105.132240 1.983772 -81.348038 0 0 31489 0.00 -0.386049 9.414050 -2.555704 -0.001656 0.002078 0.014735 0.047267 0.629639 -0.650328 105.132401 1.974043 -81.346710 0 0 31490 0.00 -0.371030 9.436790 -2.570802 0.010843 0.016542 0.012881 0.046546 0.627936 -0.648043 105.139542 1.962945 -81.336380 0 0 31491 0.00 -0.355516 9.421852 -2.540348 0.025403 -0.001382 0.012697 0.046266 0.628779 -0.651189 105.155144 1.954874 -81.336662 0 0 31492 0.00 -0.355516 9.421852 -2.540348 0.014513 0.012961 -0.001424 0.046827 0.629092 -0.647466 105.164391 1.952219 -81.326546 0 0 31493 0.00 -0.332370 9.406958 -2.532852 0.032711 -0.008536 -0.006997 0.047130 0.628484 -0.650619 105.184143 1.956113 -81.327835 0 0 31494 0.00 -0.309459 9.407099 -2.586424 0.020137 -0.017582 0.002005 0.045535 0.629381 -0.649324 105.196022 1.956144 -81.336517 0 0 31495 0.00 -0.309587 9.422235 -2.525071 0.021968 -0.024786 0.016227 0.048275 0.630199 -0.650900 105.209190 1.949621 -81.350281 0 0 31496 0.00 -0.310059 9.452306 -2.647208 0.021830 -0.010367 0.016275 0.045970 0.627373 -0.647186 105.222099 1.940680 -81.355507 0 0 31497 0.00 -0.348240 9.452073 -2.555371 0.021970 -0.025685 0.012665 0.045702 0.625044 -0.649772 105.235275 1.936264 -81.369232 0 0 31498 0.00 -0.355975 9.451936 -2.647182 -0.003260 -0.028494 0.016454 0.045396 0.628802 -0.649755 105.233475 1.929956 -81.385612 0 0 31499 0.00 -0.355934 9.451973 -2.601274 -0.004938 -0.042905 0.012863 0.047124 0.628782 -0.649472 105.230911 1.928039 -81.408897 0 0 31500 0.00 -0.310039 9.452325 -2.624254 0.002076 -0.015866 0.005744 0.046687 0.628514 -0.647755 105.232460 1.925749 -81.414589 0 0 31501 0.00 -0.294481 9.429801 -2.647429 0.000137 0.002125 0.007591 0.048141 0.628749 -0.651765 105.233673 1.919953 -81.412178 0 0 31502 0.00 -0.309514 9.407048 -2.647634 0.005628 -0.005046 -0.003174 0.046397 0.629663 -0.648895 105.237495 1.920965 -81.412361 0 0 31503 0.00 -0.340279 9.421912 -2.616869 -0.001568 -0.012296 0.017370 0.046846 0.627762 -0.651051 105.237419 1.911934 -81.419395 0 0 31504 0.00 -0.294000 9.392111 -2.617180 0.012880 -0.012213 0.005649 0.046396 0.629236 -0.648181 105.245224 1.909148 -81.424492 0 0 31505 0.00 -0.301820 9.407148 -2.601731 0.011088 -0.015826 0.012786 0.046985 0.627772 -0.649620 105.252357 1.903168 -81.432785 0 0 31506 0.00 -0.309696 9.422134 -2.647492 0.003922 -0.019450 0.000368 0.046406 0.627214 -0.648189 105.254921 1.904393 -81.441147 0 0 31507 0.00 -0.340488 9.436973 -2.647332 -0.003307 -0.015892 -0.004011 0.046418 0.627045 -0.651053 105.253899 1.907711 -81.446945 0 0 31508 0.00 -0.332297 9.391770 -2.655415 0.014781 -0.022996 -0.005089 0.046116 0.627509 -0.647901 105.262642 1.912488 -81.456390 0 0 31509 0.00 -0.309366 9.391931 -2.686033 0.018375 -0.022968 -0.003339 0.046416 0.627762 -0.651623 105.273911 1.916506 -81.466202 0 0 31510 0.00 -0.309568 9.406998 -2.708844 0.021981 -0.022944 -0.008716 0.045549 0.626353 -0.648907 105.286804 1.923284 -81.475449 0 0 31511 0.00 -0.264198 9.452626 -2.708444 0.025508 -0.015721 -0.005160 0.045272 0.627044 -0.652912 105.302307 1.927199 -81.480972 0 0 31512 0.00 -0.241115 9.445300 -2.670272 0.009115 0.007584 -0.001386 0.043964 0.626371 -0.649190 105.308350 1.925313 -81.475388 0 0 31513 0.00 -0.264429 9.475292 -2.662323 0.003645 0.016550 -0.006655 0.046131 0.627188 -0.651625 105.311935 1.925130 -81.462837 0 0 31514 0.00 -0.294572 9.437344 -2.647358 0.003590 0.021934 0.007615 0.045974 0.627220 -0.648188 105.315033 1.916096 -81.447891 0 0 31515 0.00 -0.355793 9.436850 -2.647324 -0.003602 0.023689 -0.004790 0.047859 0.627310 -0.651627 105.314583 1.913801 -81.431671 0 0 31516 0.00 -0.370853 9.414072 -2.678133 0.003764 0.003037 -0.004914 0.045837 0.626348 -0.649051 105.317497 1.914551 -81.427185 0 0 31517 0.00 -0.385649 9.376285 -2.617270 0.014662 -0.005021 -0.006823 0.047292 0.625441 -0.651634 105.327003 1.917757 -81.426537 0 0 31518 0.00 -0.370667 9.406617 -2.571086 0.012789 0.002159 0.000345 0.045396 0.627516 -0.648186 105.335045 1.915733 -81.423111 0 0 31519 0.00 -0.309850 9.437245 -2.616745 0.009006 0.021953 0.005783 0.047858 0.627741 -0.651912 105.341736 1.907891 -81.409470 0 0 31520 0.00 -0.309907 9.444820 -2.578417 0.007257 0.018341 -0.004906 0.046554 0.626632 -0.648478 105.346939 1.906313 -81.395531 0 0 31521 0.00 -0.347750 9.406765 -2.617007 0.016320 0.012988 -0.007677 0.046134 0.626611 -0.651627 105.357719 1.907264 -81.384796 0 0 31522 0.00 -0.363223 9.421740 -2.601554 0.006258 0.029123 0.005827 0.046130 0.626904 -0.651053 105.362488 1.898117 -81.367981 0 0 31523 0.00 -0.355598 9.421776 -2.632163 -0.000018 0.027303 -0.004814 0.046705 0.627756 -0.651910 105.364159 1.895331 -81.349770 0 0 31524 0.00 -0.371169 9.444288 -2.624290 0.003627 0.020118 -0.001300 0.047279 0.626899 -0.649910 105.367294 1.891486 -81.335220 0 0 31525 0.00 -0.355779 9.436862 -2.632021 -0.003529 0.009288 0.012993 0.047862 0.627589 -0.652771 105.366531 1.881618 -81.329674 0 0 31526 0.00 -0.371071 9.436751 -2.616710 0.012712 0.006664 0.012839 0.046114 0.628940 -0.649470 105.374550 1.872005 -81.326523 0 0 31527 0.00 -0.393952 9.429010 -2.632071 -0.004453 0.012874 0.013012 0.047868 0.626149 -0.652348 105.373329 1.861616 -81.319008 0 0 31528 0.00 -0.355611 9.421763 -2.647466 0.002055 -0.014073 0.012878 0.048428 0.627035 -0.649196 105.374870 1.855131 -81.324684 0 0 31529 0.00 -0.324833 9.406912 -2.662928 -0.001732 0.012909 0.004072 0.047583 0.625859 -0.652921 105.375252 1.849689 -81.315788 0 0 31530 0.00 -0.309548 9.407017 -2.685890 -0.003573 0.017406 0.004102 0.046994 0.626038 -0.649770 105.374176 1.843271 -81.305855 0 0 31531 0.00 -0.278574 9.377092 -2.686192 -0.017901 0.012846 -0.017173 0.049018 0.626712 -0.652348 105.365402 1.849569 -81.293770 0 0 31532 0.00 -0.271096 9.392246 -2.678403 -0.007118 0.016499 -0.018151 0.048138 0.627900 -0.649764 105.362381 1.855584 -81.278496 0 0 31533 0.00 -0.309682 9.422147 -2.632189 0.003805 0.003944 -0.026303 0.048448 0.625991 -0.653066 105.365936 1.868263 -81.269943 0 0 31534 0.00 -0.356150 9.467028 -2.639388 -0.014251 0.005646 -0.021673 0.046417 0.627190 -0.651052 105.358658 1.877873 -81.262505 0 0 31535 0.00 -0.348195 9.436861 -2.708539 -0.012489 0.007466 -0.010099 0.048726 0.627581 -0.652487 105.352867 1.881087 -81.254463 0 0 31536 0.00 -0.309568 9.406998 -2.708844 -0.017906 0.010145 -0.010938 0.047856 0.627034 -0.650197 105.343521 1.884084 -81.243622 0 0 31537 0.00 -0.294418 9.422233 -2.678106 -0.025008 -0.005189 -0.006460 0.047870 0.625715 -0.652493 105.330315 1.887200 -81.243134 0 0 31538 0.00 -0.279294 9.437442 -2.677972 -0.014337 0.012861 -0.006506 0.047135 0.625902 -0.648625 105.323044 1.887341 -81.233116 0 0 31539 0.00 -0.279099 9.422369 -2.662812 -0.025200 0.023602 -0.017074 0.049020 0.626420 -0.652635 105.310310 1.891941 -81.215096 0 0 31540 0.00 -0.293936 9.384543 -2.647856 -0.021710 0.045209 -0.033092 0.047559 0.627772 -0.648762 105.299545 1.901886 -81.182442 0 0 31541 0.00 -0.309269 9.384394 -2.678452 -0.014675 0.061435 -0.010829 0.047714 0.627172 -0.651198 105.293503 1.897312 -81.144447 0 0 31542 0.00 -0.339970 9.391690 -2.678364 -0.025391 0.048781 -0.011657 0.047562 0.627193 -0.648907 105.280586 1.894881 -81.113861 0 0 31543 0.00 -0.309269 9.384394 -2.678452 -0.016306 0.039836 -0.015330 0.048718 0.629026 -0.652338 105.273239 1.896074 -81.087135 0 0 31544 0.00 -0.248334 9.407504 -2.693577 -0.036225 0.048747 -0.006212 0.047844 0.628060 -0.648475 105.254089 1.890651 -81.056953 0 0 31545 0.00 -0.187154 9.407961 -2.739519 -0.009275 0.063301 -0.025131 0.049431 0.628892 -0.650049 105.251251 1.893680 -81.015762 0 0 31546 0.00 -0.217959 9.422787 -2.754662 0.008468 0.097572 -0.018956 0.050587 0.627157 -0.648627 105.258659 1.887945 -80.955162 0 0 31547 0.00 -0.217441 9.377503 -2.785694 -0.007806 0.108294 -0.025912 0.048724 0.627442 -0.651772 105.257484 1.884566 -80.888962 0 0 31548 0.00 -0.248045 9.377263 -2.778025 -0.007817 0.110086 -0.025906 0.050870 0.628022 -0.648337 105.255814 1.880785 -80.822296 0 0 31549 0.00 -0.278790 9.392146 -2.724306 -0.002485 0.123594 -0.036611 0.051745 0.628130 -0.651202 105.258026 1.880992 -80.746017 0 0 31550 0.00 -0.332344 9.391726 -2.708974 0.005551 0.133517 -0.034874 0.051736 0.628007 -0.648769 105.264481 1.878629 -80.664833 0 0 31551 0.00 -0.401345 9.406307 -2.647582 -0.008838 0.128019 -0.024063 0.052192 0.625379 -0.651500 105.263069 1.871256 -80.588005 0 0 31552 0.00 -0.386047 9.406425 -2.655242 0.001180 0.115480 -0.031318 0.052180 0.626121 -0.649207 105.266663 1.869644 -80.517769 0 0 31553 0.00 -0.386390 9.436615 -2.632004 -0.013259 0.120805 -0.041865 0.053624 0.626951 -0.651210 105.262688 1.873240 -80.442253 0 0 31554 0.00 -0.401191 9.391196 -2.678329 -0.000503 0.102881 -0.042032 0.052889 0.627279 -0.647772 105.265144 1.879451 -80.376625 0 0 31555 0.00 -0.370641 9.391386 -2.747208 0.001249 0.108307 -0.043814 0.054048 0.628106 -0.650634 105.269295 1.886054 -80.307724 0 0 31556 0.00 -0.340415 9.421785 -2.769895 -0.018539 0.102822 -0.047211 0.053026 0.629293 -0.648336 105.261459 1.895135 -80.241829 0 0 31557 0.00 -0.355888 9.436761 -2.754442 -0.018652 0.115409 -0.039154 0.054904 0.629543 -0.650057 105.254349 1.898128 -80.169708 0 0 31558 0.00 -0.401609 9.421317 -2.739255 -0.016748 0.106413 -0.050782 0.054330 0.628261 -0.648916 105.247643 1.908658 -80.100739 0 0 31559 0.00 -0.432199 9.421089 -2.716284 -0.018456 0.091997 -0.041894 0.056932 0.628494 -0.651496 105.240257 1.916774 -80.041168 0 0 31560 0.00 -0.462621 9.405763 -2.708758 -0.005900 0.099248 -0.036642 0.055190 0.627403 -0.646630 105.239578 1.920579 -79.978172 0 0 31561 0.00 -0.447147 9.390787 -2.724211 0.006789 0.084919 -0.020756 0.056354 0.628220 -0.650637 105.246452 1.918160 -79.925705 0 0 31562 0.00 -0.416328 9.375974 -2.693765 -0.004013 0.088467 -0.034020 0.056347 0.628236 -0.648776 105.246651 1.922134 -79.869247 0 0 31563 0.00 -0.423967 9.375925 -2.678458 0.002377 0.079499 -0.040341 0.056355 0.628358 -0.651353 105.251015 1.931412 -79.816833 0 0 31564 0.00 -0.401073 9.383678 -2.647795 0.023176 0.072406 -0.050353 0.056058 0.627670 -0.647919 105.266586 1.946824 -79.767227 0 0 31565 0.00 -0.385683 9.376252 -2.655526 0.015984 0.070575 -0.051185 0.057803 0.626611 -0.650933 105.278679 1.963459 -79.718109 0 0 31566 0.00 -0.370399 9.376357 -2.678489 0.026788 0.070636 -0.049500 0.057361 0.626925 -0.648640 105.296310 1.978641 -79.668663 0 0 31567 0.00 -0.400659 9.345925 -2.694058 0.024959 0.078724 -0.061939 0.057806 0.626033 -0.650935 105.313797 1.999992 -79.613403 0 0 31568 0.00 -0.447016 9.383283 -2.678375 0.015973 0.070567 -0.047617 0.057211 0.627940 -0.648350 105.325249 2.014117 -79.564980 0 0 31569 0.00 -0.462439 9.390676 -2.708900 0.025027 0.064319 -0.049496 0.059103 0.626874 -0.651937 105.342476 2.030817 -79.519569 0 0 31570 0.00 -0.432010 9.406010 -2.708775 -0.003695 0.047086 -0.043045 0.057792 0.627065 -0.648498 105.342201 2.045956 -79.484444 0 0 31571 0.00 -0.416782 9.413689 -2.693410 0.008993 0.039955 -0.052982 0.057662 0.626464 -0.651363 105.349823 2.068313 -79.451973 0 0 31572 0.00 -0.447379 9.413454 -2.678090 0.001695 0.052505 -0.052881 0.057371 0.626189 -0.650218 105.352821 2.088060 -79.413010 0 0 31573 0.00 -0.431969 9.406048 -2.662867 0.003586 0.041719 -0.054712 0.058383 0.626882 -0.652078 105.357430 2.111149 -79.379303 0 0 31574 0.00 -0.477676 9.390616 -2.632378 0.021505 0.056187 -0.053054 0.058664 0.626324 -0.649361 105.371887 2.130422 -79.336922 0 0 31575 0.00 -0.538954 9.397696 -2.594016 0.001834 0.034476 -0.044023 0.058536 0.626146 -0.653513 105.375313 2.148774 -79.308846 0 0 31576 0.00 -0.538765 9.382617 -2.586507 0.029046 0.013020 -0.051459 0.057222 0.626345 -0.649072 105.393211 2.173714 -79.292099 0 0 31577 0.00 -0.493129 9.405610 -2.593971 0.018526 -0.030209 -0.040787 0.057955 0.625593 -0.651510 105.404854 2.200185 -79.300270 0 0 31578 0.00 -0.401604 9.428948 -2.632066 0.015001 -0.039194 -0.054147 0.056645 0.626068 -0.648643 105.413620 2.234551 -79.310997 0 0 31579 0.00 -0.340242 9.414319 -2.678151 0.016566 -0.012179 -0.040720 0.056943 0.625469 -0.650650 105.424515 2.258228 -79.309204 0 0 31580 0.00 -0.332708 9.421898 -2.708689 0.016452 0.000422 -0.035336 0.056942 0.624188 -0.648508 105.434860 2.276170 -79.300766 0 0 31581 0.00 -0.386249 9.421492 -2.678054 0.014571 0.012992 -0.038848 0.057240 0.625446 -0.652941 105.445160 2.294952 -79.285332 0 0 31582 0.00 -0.455263 9.436059 -2.631965 0.003654 0.023708 -0.024459 0.055788 0.625489 -0.650075 105.448624 2.303331 -79.266808 0 0 31583 0.00 -0.493533 9.435744 -2.639595 0.001829 0.027293 -0.026214 0.056520 0.625167 -0.652798 105.451881 2.312989 -79.245399 0 0 31584 0.00 -0.463279 9.466169 -2.631676 0.000103 0.012892 -0.015542 0.056654 0.624904 -0.649650 105.453018 2.318092 -79.233025 0 0 31585 0.00 -0.478612 9.466021 -2.662273 -0.005274 0.006569 -0.008380 0.057823 0.624282 -0.653090 105.451637 2.321097 -79.225800 0 0 31586 0.00 -0.478151 9.428312 -2.654977 0.018172 0.007585 -0.015723 0.054924 0.625357 -0.649931 105.463013 2.327111 -79.217850 0 0 31587 0.00 -0.470323 9.413281 -2.662775 0.018208 0.002189 -0.012175 0.056077 0.626627 -0.651646 105.475021 2.332916 -79.212471 0 0 31588 0.00 -0.432115 9.413540 -2.724007 -0.000723 0.003014 -0.015564 0.056211 0.627648 -0.650210 105.475464 2.339537 -79.205132 0 0 31589 0.00 -0.416739 9.406101 -2.747040 0.002807 0.010235 -0.007556 0.055637 0.627648 -0.651068 105.478813 2.341573 -79.196014 0 0 31590 0.00 -0.385940 9.391269 -2.739548 -0.006122 0.003900 -0.020863 0.055632 0.627662 -0.649493 105.476219 2.350986 -79.188530 0 0 31591 0.00 -0.371139 9.436687 -2.693223 0.003469 0.043525 -0.013709 0.056526 0.624154 -0.653088 105.480743 2.351310 -79.160072 0 0 31592 0.00 -0.371266 9.451824 -2.631871 -0.007265 0.030862 -0.002953 0.056514 0.625040 -0.650794 105.477989 2.346710 -79.140198 0 0 31593 0.00 -0.371044 9.436777 -2.586105 0.003636 0.020111 -0.001302 0.057812 0.625876 -0.652368 105.481987 2.343730 -79.126572 0 0 31594 0.00 -0.416785 9.421314 -2.593872 -0.003527 0.012869 0.005872 0.056214 0.625926 -0.648929 105.480919 2.337007 -79.118103 0 0 31595 0.00 -0.424639 9.436319 -2.616680 -0.001844 0.029076 0.000557 0.057241 0.624873 -0.652371 105.481964 2.331627 -79.099808 0 0 31596 0.00 -0.493492 9.435782 -2.593687 -0.003583 0.020051 0.005896 0.056506 0.625630 -0.649360 105.481018 2.323792 -79.087395 0 0 31597 0.00 -0.508246 9.390408 -2.586453 -0.005140 -0.012351 0.012946 0.058542 0.624703 -0.653376 105.479172 2.317953 -79.093895 0 0 31598 0.00 -0.492577 9.360359 -2.586746 -0.013913 -0.044782 0.020062 0.056511 0.625476 -0.650506 105.470772 2.312209 -79.119423 0 0 31599 0.00 -0.477697 9.390597 -2.655332 -0.010151 -0.069937 0.024420 0.057811 0.626880 -0.653223 105.464699 2.308876 -79.159508 0 0 31600 0.00 -0.416637 9.406197 -2.632271 -0.000987 -0.086074 0.007359 0.056798 0.626046 -0.650934 105.462860 2.316449 -79.205215 0 0 31601 0.00 -0.385831 9.391370 -2.617128 -0.013663 -0.082541 0.027087 0.057665 0.626884 -0.652936 105.454475 2.313554 -79.252670 0 0 31602 0.00 -0.385495 9.361173 -2.648017 -0.019131 -0.071765 0.020035 0.054630 0.626659 -0.650068 105.442490 2.311932 -79.293816 0 0 31603 0.00 -0.370058 9.353791 -2.602189 -0.024703 -0.048408 0.020147 0.057517 0.627039 -0.651933 105.428574 2.307625 -79.321342 0 0 31604 0.00 -0.354844 9.361458 -2.602127 -0.012056 -0.053740 0.021800 0.057516 0.625899 -0.650220 105.421036 2.302264 -79.350159 0 0 31605 0.00 -0.355564 9.421808 -2.593907 -0.015700 -0.053762 0.032533 0.056661 0.626174 -0.653080 105.412086 2.291886 -79.382523 0 0 31606 0.00 -0.371434 9.466923 -2.616426 -0.010283 -0.059132 0.038713 0.055206 0.627508 -0.651211 105.405350 2.277995 -79.419968 0 0 31607 0.00 -0.370903 9.421653 -2.632155 0.007839 -0.068934 0.030498 0.056661 0.626744 -0.653937 105.409569 2.271023 -79.460403 0 0 31608 0.00 -0.370714 9.406573 -2.624645 0.004162 -0.055456 0.019872 0.054487 0.626373 -0.649926 105.411316 2.266980 -79.491791 0 0 31609 0.00 -0.401786 9.444035 -2.631924 -0.006663 -0.057315 0.027099 0.056219 0.627770 -0.652786 105.407501 2.260106 -79.525284 0 0 31610 0.00 -0.386767 9.466774 -2.647022 0.005907 -0.051847 0.023438 0.055204 0.626371 -0.649068 105.410316 2.253543 -79.554405 0 0 31611 0.00 -0.371489 9.466872 -2.677636 0.007635 -0.040132 0.014544 0.056229 0.626463 -0.653651 105.415146 2.250976 -79.576485 0 0 31612 0.00 -0.355470 9.406640 -2.693516 0.000486 -0.046460 0.016367 0.053338 0.625950 -0.650498 105.415016 2.247502 -79.603355 0 0 31613 0.00 -0.347804 9.406714 -2.678218 0.011309 -0.048208 0.018046 0.054632 0.627082 -0.651212 105.421761 2.244208 -79.630432 0 0 31614 0.00 -0.339879 9.384147 -2.678435 0.012925 -0.023009 0.019881 0.055352 0.626789 -0.650641 105.429245 2.235224 -79.642448 0 0 31615 0.00 -0.355234 9.391604 -2.632448 -0.001416 -0.030287 0.012861 0.056517 0.626461 -0.653508 105.429115 2.232039 -79.658829 0 0 31616 0.00 -0.325128 9.437147 -2.586131 0.011215 -0.033826 0.013630 0.055349 0.626939 -0.650068 105.435425 2.228159 -79.676987 0 0 31617 0.00 -0.279926 9.497874 -2.570286 0.013948 -0.037402 0.003797 0.054217 0.625904 -0.654508 105.443985 2.231004 -79.695915 0 0 31618 0.00 -0.279771 9.482762 -2.601033 0.009306 -0.025729 0.027041 0.054055 0.626378 -0.650068 105.449303 2.218487 -79.712540 0 0 31619 0.00 -0.340824 9.467170 -2.616443 -0.004348 -0.005113 0.021875 0.054642 0.626773 -0.653647 105.447952 2.206367 -79.716370 0 0 31620 0.00 -0.431915 9.406098 -2.601657 0.018315 -0.017614 0.012719 0.054630 0.627230 -0.650781 105.458687 2.200521 -79.725388 0 0 31621 0.00 -0.492850 9.382988 -2.586533 0.023967 -0.047288 0.007238 0.055657 0.625176 -0.653082 105.472763 2.202971 -79.750298 0 0 31622 0.00 -0.431942 9.406073 -2.632262 0.004106 -0.042867 0.002085 0.054350 0.624075 -0.648790 105.474884 2.206861 -79.771713 0 0 31623 0.00 -0.401359 9.406295 -2.662885 0.000361 -0.024880 0.002169 0.054502 0.626051 -0.653792 105.475929 2.208704 -79.783463 0 0 31624 0.00 -0.402045 9.466676 -2.616408 0.014876 -0.041012 0.007345 0.053920 0.626072 -0.652216 105.484230 2.209409 -79.805130 0 0 31625 0.00 -0.432773 9.473947 -2.646925 -0.010340 -0.047438 0.021817 0.055082 0.625322 -0.653796 105.478554 2.203866 -79.832359 0 0 31626 0.00 -0.386222 9.421516 -2.647449 0.004084 -0.044657 0.014558 0.054206 0.625218 -0.650359 105.480553 2.201144 -79.856346 0 0 31627 0.00 -0.363089 9.406610 -2.655255 -0.003047 -0.054584 0.014594 0.054217 0.625191 -0.653509 105.478943 2.200674 -79.886414 0 0 31628 0.00 -0.355679 9.421700 -2.723979 -0.001366 -0.041065 0.016402 0.052904 0.626244 -0.650496 105.477882 2.196385 -79.909729 0 0 31629 0.00 -0.340919 9.467081 -2.723561 -0.003170 -0.039268 0.003950 0.053210 0.625342 -0.654222 105.476601 2.199429 -79.929703 0 0 31630 0.00 -0.356581 9.497136 -2.715617 -0.013941 -0.044723 0.000471 0.053781 0.622780 -0.649080 105.468353 2.204493 -79.951309 0 0 31631 0.00 -0.333239 9.467169 -2.692960 -0.010305 -0.051907 0.016456 0.053495 0.625919 -0.653934 105.462631 2.202533 -79.980179 0 0 31632 0.00 -0.340313 9.421881 -2.655126 -0.026364 -0.066388 0.002296 0.051177 0.626548 -0.651350 105.446793 2.209891 -80.016098 0 0 31633 0.00 -0.386074 9.406399 -2.685847 -0.006460 -0.077087 0.002087 0.053783 0.626200 -0.654363 105.442810 2.219684 -80.056686 0 0 31634 0.00 -0.401386 9.406269 -2.693490 -0.001040 -0.084263 0.020734 0.051608 0.625974 -0.650351 105.440979 2.219578 -80.103180 0 0 31635 0.00 -0.401177 9.391209 -2.663027 -0.010140 -0.071721 0.023522 0.052049 0.626518 -0.653500 105.434883 2.216720 -80.144073 0 0 31636 0.00 -0.416651 9.406183 -2.647573 -0.015559 -0.069954 0.022686 0.051607 0.625406 -0.649209 105.425034 2.213345 -80.183365 0 0 31637 0.00 -0.401709 9.436479 -2.647298 -0.020958 -0.069975 0.014717 0.051758 0.625958 -0.651927 105.412834 2.215083 -80.221954 0 0 31638 0.00 -0.355870 9.444406 -2.631950 -0.020961 -0.071771 0.021841 0.051316 0.625559 -0.648635 105.399857 2.212435 -80.262283 0 0 31639 0.00 -0.340642 9.452085 -2.616585 -0.019218 -0.065466 0.027189 0.051612 0.625965 -0.651354 105.388664 2.206553 -80.300270 0 0 31640 0.00 -0.355611 9.421763 -2.647466 -0.012068 -0.054629 0.018241 0.050442 0.627731 -0.649197 105.381172 2.203273 -80.331039 0 0 31641 0.00 -0.371007 9.429183 -2.647386 -0.035375 -0.069141 0.013066 0.050752 0.625252 -0.651641 105.360733 2.205722 -80.368912 0 0 31642 0.00 -0.355598 9.421776 -2.632163 -0.038930 -0.073656 0.007737 0.049592 0.625996 -0.650777 105.337509 2.211112 -80.408752 0 0 31643 0.00 -0.340511 9.444579 -2.570749 -0.019097 -0.076267 0.012897 0.050173 0.626549 -0.652780 105.326233 2.214682 -80.450539 0 0 31644 0.00 -0.294558 9.437356 -2.632056 -0.019126 -0.077149 0.025372 0.050588 0.627726 -0.649627 105.314171 2.210835 -80.493401 0 0 31645 0.00 -0.309696 9.422134 -2.647492 -0.017383 -0.069944 0.028940 0.049588 0.628003 -0.652487 105.303917 2.204515 -80.534111 0 0 31646 0.00 -0.309527 9.407036 -2.662937 -0.029917 -0.076298 0.014776 0.046980 0.626928 -0.647046 105.285759 2.206378 -80.577774 0 0 31647 0.00 -0.355093 9.376481 -2.678498 -0.013820 -0.059130 0.014676 0.049582 0.628588 -0.651625 105.277855 2.206262 -80.610344 0 0 31648 0.00 -0.401136 9.391247 -2.617119 0.002409 -0.059069 0.012748 0.048850 0.628482 -0.648189 105.278595 2.206631 -80.641090 0 0 31649 0.00 -0.431552 9.375926 -2.601941 -0.006478 -0.075317 0.016347 0.047720 0.627016 -0.652487 105.274551 2.208052 -80.682869 0 0 31650 0.00 -0.332095 9.376704 -2.632603 0.002516 -0.073447 0.012704 0.046833 0.628506 -0.648471 105.275040 2.210614 -80.723770 0 0 31651 0.00 -0.263423 9.392326 -2.655453 0.015124 -0.071565 0.003684 0.047709 0.627899 -0.650622 105.283516 2.218420 -80.761551 0 0 31652 0.00 -0.232974 9.407679 -2.632375 -0.001288 -0.051858 0.024384 0.046114 0.628513 -0.648756 105.282219 2.211272 -80.791595 0 0 31653 0.00 -0.263585 9.407432 -2.632357 0.016795 -0.051767 -0.005188 0.046420 0.627897 -0.652767 105.292114 2.220914 -80.817078 0 0 31654 0.00 -0.271069 9.392271 -2.647798 0.006718 -0.028423 -0.008598 0.046696 0.627064 -0.648477 105.296097 2.228458 -80.828415 0 0 31655 0.00 -0.293859 9.376987 -2.663229 0.002200 -0.030250 0.005697 0.046130 0.626904 -0.651053 105.298019 2.228779 -80.843636 0 0 31656 0.00 -0.247930 9.377371 -2.647953 0.003941 -0.021239 0.003030 0.045405 0.626782 -0.649621 105.300491 2.228812 -80.854149 0 0 31657 0.00 -0.225140 9.392654 -2.632521 0.007437 -0.005024 -0.004977 0.046572 0.627020 -0.653773 105.306007 2.231132 -80.853790 0 0 31658 0.00 -0.233183 9.422739 -2.662838 0.000165 -0.001459 0.005797 0.046700 0.626627 -0.648908 105.306732 2.226644 -80.852234 0 0 31659 0.00 -0.278903 9.407295 -2.647651 0.003546 0.030935 0.000508 0.047861 0.627165 -0.651771 105.310753 2.220419 -80.832809 0 0 31660 0.00 -0.370449 9.383938 -2.632510 -0.003637 0.030880 -0.004775 0.046698 0.626489 -0.648193 105.310051 2.216882 -80.812775 0 0 31661 0.00 -0.370526 9.391494 -2.617136 0.000025 0.023698 -0.006610 0.046430 0.626588 -0.653775 105.311935 2.215680 -80.796272 0 0 31662 0.00 -0.401298 9.406351 -2.594023 0.016315 0.020176 -0.028154 0.046415 0.626623 -0.649766 105.322571 2.226680 -80.778778 0 0 31663 0.00 -0.370849 9.421703 -2.570944 0.003611 0.030909 -0.024445 0.048437 0.627728 -0.652629 105.326775 2.234237 -80.755592 0 0 31664 0.00 -0.340258 9.421931 -2.593915 0.008888 0.045338 -0.017324 0.046985 0.628202 -0.650047 105.333641 2.235436 -80.725250 0 0 31665 0.00 -0.355725 9.436913 -2.570811 0.001690 0.043496 -0.015480 0.047576 0.627445 -0.653201 105.336960 2.236103 -80.696449 0 0 31666 0.00 -0.355466 9.414271 -2.586327 0.017941 0.041782 -0.022763 0.047287 0.626024 -0.650916 105.348969 2.240840 -80.667679 0 0 31667 0.00 -0.340224 9.421963 -2.555659 0.010781 0.038147 -0.031621 0.049013 0.627723 -0.652344 105.357468 2.251201 -80.639389 0 0 31668 0.00 -0.355732 9.436907 -2.578462 -0.003787 0.057869 -0.033215 0.046991 0.627187 -0.650481 105.357452 2.259265 -80.600182 0 0 31669 0.00 -0.355843 9.444430 -2.601345 0.012323 0.072349 -0.036884 0.049016 0.626432 -0.651347 105.367615 2.267314 -80.552170 0 0
Regards,
Hi Kazola,
IAR is specified a development platform for CC2540 and other CC family products.
I have learned a practical embedded processor subject using Zilog Microcontroller, however, my coding skills are still weak.
What other platforms can use?
Regards,
For CC2540, I think the only thing you can use is IAR.
If you use CC2540 as a BLE Network Processor, you can use whatever OS where you can program a serial application capable to send HCI, similar to AT-commands.
For other things that are not transceivers, like for example microcontrolers as the MSP430, the CodeComposer software also exists, which I thing it is based on Eclipse IDE.
Bye!
Hi Kazola,
I have two academic semesters of embedded C programming although the applications are not independently done by me. I think I'd better use the free evaluation IAR to do it within one month.
Can I ask you how to start in C? How to use the "fread" function to load my data file first then I can buffer the data and start considerring how to send it?
Regards,