Tool/software:
I need Implement multi-byte notify based on single byte notify, the single byte notify based on basic_ble_LP_EM_CC2340R5_freertos_ticlang, can anyone help me?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Peter,
Thank you for reaching out! If I'm understanding correctly, you'd like to increase the number of bytes sent out by the notification, inside the basic_ble example.
If that's the case, the fix should be relatively easy, as this is a commonly asked question!
Ultimately, if you're using the GATTServApp_ProcessCharCfg() function, the function will lead to theSimpleGattProfile_readAttrCB callback. In the out of box example, the callback only manages 1 byte as seen below:
*pLen = 1;
pValue[0] = *pAttr->pValue;
however, simply changing this to a memcpy, as seen below, should fix the issue.
*plen = x; // where x is the number of bytes memcpy(pValue, pAttr->pValue, x);
I hope this helps! If this doesn't fix the issue, please provide me with more details regarding what you're seeing and I'll make sure to help!
Best Regards,
Tarek D