This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2340R5: using Mcuboot,presisent and application if we do the reset it is happening in 4-5 sec

Part Number: CC2340R5


Tool/software:

HI team,

We are working with the CC2340R5 using SDK 8.40 and IDE 12.8. We're facing an issue where

  • when running with mcuboot_onchip, persistent, and application (OAD) images, a reset takes approximately 4–5 seconds.

  • If we run only the mcuboot_onchip, application layer, a device reset takes around 300–400 milliseconds.

why the behavior is different from this above two steps.

Can you give some suggestions, which is useful for our understanding and further development.

Thanks and regards

chandra shekar