Part Number: LAUNCHXL-CC26X2R1
Tool/software:
How can I use the parameters obtained from the command to calculate the “HCI_EXT_PacketErrorRateCmd()” command PER?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: LAUNCHXL-CC26X2R1
Tool/software:
How can I use the parameters obtained from the command to calculate the “HCI_EXT_PacketErrorRateCmd()” command PER?
Hi !
The documentation about the HCI_EXT_PacketErrorRateCmd function is a bit evasive, I agree.
You can recieve the message from by first registering with GAP for HCI/Host messages with the GAP_RegisterForMsgs(selfEntity), and then call HCI_EXT_PacketErrorRateCmd (See user guide for more details).
Then, your function that processes stack messages (for example, the function SimplePeripheral_processStackMsg in the Simple Peripheral project) will recieve the HCI message. You can filter for the right message by checking if your message have the right event (HCI_GAP_EVENT_EVENT), that have the right status (HCI_VE_EVENT_CODE) and the right cmdOpcode (HCI_EXT_PER) when casted to hciEvt_CommandStatus_t.
The format of the message is the following :
- 8 bytes of the LSB of EventOpcode (the opcode should be HCI_EXT_PER_EVENT)
- 8 bytes of the MSB of EventOpcode (the opcode should be HCI_EXT_PER_EVENT)
- 8 bytes of the status (should be HCI_SUCCESS)
- 8 bytes of the command (should be HCI_EXT_PER_READ)
- 8 bytes of the LSB of the number of packets
- 8 bytes of the MSB of the number of packets
- 8 bytes of the LSB of the number of CRC errors
- 8 bytes of the MSB of the number of CRC errors
- 8 bytes of the LSB of the number of events
- 8 bytes of the MSB of the number of events
- 8 bytes of the MSB of the number of missed events
- 8 bytes of the LSB of the number of missed events
Could you try if this corresponds to the data you expect ? Could you also tell me if you recieve one or two events from calling once the HCI_EXT_PacketErrorRateCmd function ?
Kind regards,
Maxence
Hi Maxence
Thanks for your reply.
I understood that I get the message with HCI_EXT_PER. Thank you very much for your kindness.
> Could you try if this corresponds to the data you expect ?
Here is the data I expected.
> ould you also tell me if you recieve one or two events from calling once the HCI_EXT_PacketErrorRateCmd function ?
One event occurred.
I can get the number of CRC errors and the number of packets received from the message content in HCI_EXT_PER, but which of these parameters can I use to find the value of PER?
Is it simply “CRC errors / number of packets”?
Best regards
Hi !
Yes, “CRC errors / number of packets” is the formula to compute the packet error rate.
Kind regards,
Maxence