Part Number: CC2652R
Other Parts Discussed in Thread: LAUNCHXL-CC26X2R1
Tool/software:
Dear Team,
The customer requested a sample or demo source code for connecting with Windows 11.
Can TI provide it for the cutomer?
Thanks and Regards,
Hara
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: CC2652R
Other Parts Discussed in Thread: LAUNCHXL-CC26X2R1
Tool/software:
Dear Team,
The customer requested a sample or demo source code for connecting with Windows 11.
Can TI provide it for the cutomer?
Thanks and Regards,
Hara
Hi Hara,
If you program e.g. basic_ble in peripheral configuration you should be able to see and connect via Windows Blutooth interface. Make sure to enable Bluetooth low energy on the Windows side.
Cheers,
Marie H
Hello Marie H
I checked if it's working basic_ble project with windows 11.
LAUNCHXL-CC26X2R1 (Eva board)
SDK 7.10.00.98 (ticlang v3.2.2 LTS)
Windws 11 (24H2) (ThinkadPad E14)
Immediately after pairing, the connection was disconnected.
Is there anything I should check first?
best regards
Hideo Toyama (Comrade Corp.)
---------- uart log
# 1 RP Addr: 0x4520853626CA
# 2 Peripheral_start: Register Handlers
# 3 Peripheral_start: Init Adv Set 1
# 4 Peripheral_start: Start Adv Set 1
# 5 Pairing_start: Register Handlers
# 6 Data_start: Register Handlers
# 7 ADV_START_AFTER_ENABLE: Peripheral role, advhandle: 0
# 8 ADV_END_AFTER_DISABLE: Peripheral role, advhandle: 0
# 9 LINK_ESTABLISHED_EVENT: Peripheral role Connected to 0xBC542FF43511, c# 10 LINK_ESTABLISHED_EVENT: Peripheral role Num Conns = 1
# 11 PAIRING_STATE_STARTED: connectionHandle = 0
# 12 PAIRING_STATE_STARTED: status = 0
# 13 PAIRING_STATE_STARTED: connectionHandle = 0
# 14 PAIRING_STATE_STARTED: status = 0
# 15 ADV_START_AFTER_ENABLE: Peripheral role, advhandle: 0
# 16 ATT_MTU_UPDATED_EVENT
# 17 PAIRING_STATE_COMPLETE: connectionHandle = 0
# 18 PAIRING_STATE_COMPLETE: status = 0
# 19 PAIRING_STATE_BOND_SAVED: connectionHandle = 0
# 20 PAIRING_STATE_BOND_SAVED: status = 0
# 21 LINK_TERMINATED_EVENT: Peripheral role, connectionHandle = 0, reason =# 22 LINK_TERMINATED_EVENT: Peripheral role, Num Conns = 0