Other Parts Discussed in Thread: UNIFLASH
Tool/software:
Hi,
I am trying to work with mcuboot bootloader which has tool to sign a binary file. The similar approach is used in the mcuboot example as well. I have been trying to flash (load) the artifact / .bin file directly from Code Composer Studio. However, I don't seem to find a way to do it. I can probably use dslite with a set target configuration in post build script. But that would mean it would load the program in the build state which I don't want to do. I went through debug config > program and load options. It does let you select other file type like .hex, .elf and .out. But there is no way to choose the *.bin file.
Note: I do know, there is also UniFlash which can do it. But, I do not want developers to have to manage two separate tools to flash it every time. Thank you in advance.