This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2745R10-Q1: [BLE 6.0 CS DKC]Python script enabling Channel Sounding function failed

Part Number: CC2745R10-Q1

Tool/software:

Hi, Ti

*SDK version: 9.11.01.09 ,example: car_node.

I used the demo code example (car_node(CC2745) & key_code(CC2340)) and only changed the UART port. However, when running the Python script, an exception occurred with the following error:

What could be causing this? Do I need any additional configuration? Because in version 9_11_00_18, it worked successfully without any modifications.

This is the sample code I used. 0488.Code.zip

Best regards!

Preston