I see nothing in the panasonic pan1326 documentation about operating in low energy mode and BRE mode simultaneously. I know that the stonestreet stack has an option to enable simultaneous operation.
We've been told that up to the point of the radio, the two modes are independent and operate simultaneously. We believe there to be a single radio shared between the two modes. How is this sharing accomplished? I would guess at some interleaving algorithm.
Specifically, can the part simultaneously maintain an A2DP stream while gathering low bandwidth data over a BLE connection?
Thanks.