Other Parts Discussed in Thread: LP-XDS110, , UNIFLASH, CC2340R5
Tool/software:
We are using LP-EM-CC2340R5 (MT-03072340R500) with LP-XDS110 (MT-0307XDS11001).
The SmartRF Studio 8 (v1.2.1) always shows the XDS110 under "Unknown/unavailable devices".
The UniFlash (8.8, 9.2) can program the device, only SmartRF Studio 8 has such issue.
When using cli.exe to print-test-targets, the XDS110 LED will immediately flash RED once, then return "Unknown (XDS110)".
We have 2 LP-XDS110 with different FW (3.0.0.36 & 3.0.0.38), both have same issue.
We have 4 different PCs with Windows 11 Home 24H2, only one PC's SmartRF can work normally.
Furthermore, we had tried to
1. remove all TI's software (drivers), and re-install SmartRF only, with Uniflash, ....
2. upgrade the windows
3.change USB ports, using power-supplied usb hub
4. upgrade the XDS110 firmware
5. install Simplelink SDK and CCS on PC
6. ......
But the issue is still the same.