Part Number: CC2745R10-Q1
Other Parts Discussed in Thread: BLE-STACK
Tool/software:
I have installed latest SDK (simplelink_lowpower_f3_sdk_9_11_00_18) for CC2745. How to read the RSSI in this SDK.
Also please share all api details for this SDK.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: CC2745R10-Q1
Other Parts Discussed in Thread: BLE-STACK
Tool/software:
I have installed latest SDK (simplelink_lowpower_f3_sdk_9_11_00_18) for CC2745. How to read the RSSI in this SDK.
Also please share all api details for this SDK.
Hello Anto,
In order to read the RSSI value in the new SDK, you need to parse the incoming message packets in your peripheral/central event handlers. If reading the RSSI value as a peripheral device, you can use the BLEAPPUTIL_SCAN_REQ_RECEIVED event mask. This will make the rssi information accessible each time the advertising device gets a scan request. Below is an example of how to access the RSSI value inside the case statement where pMsgData is a pointer to the general message struct.
case BLEAPPUTIL_SCAN_REQ_RECEIVED:
{
int rssi_value;
BLEAppUtil_AdvEventData_t* lpts_scanReqReceived = (BLEAppUtil_AdvEventData_t*)pMsgData;
rssi_value = lpts_scanReqReceived->pBuf->pScanReqRcv.rssi;
break;
}
If reading the RSSI value as a central device, you can use the BLEAPPUTIL_ADV_REPORT event mask. This will allow you to read the RSSI value of every device that is advertising around you every time an advertisement is sent.
case BLEAPPUTIL_ADV_REPORT:
{
int rssi_value;
BLEAppUtil_ScanEventData_t *scanMsg = (BLEAppUtil_ScanEventData_t *)pMsgData;
rssi_value = scanMsg->pBuf->pAdvReport.rssi;
break;
}
More information can be found here (Get RSSI from Scan Request section): Generic Access Profile (GAP) — SimpleLink Low Power F3 SDK BLE5-Stack User's Guide 9.11.00 documentation
General BLE-Stack API Documentation: TI BLE5-Stack API Documentation: BLE-Stack API Reference
Thanks,
Eshaan Tibrewala
Hello Anto,
Thank you for the clarification. There are a few ways you can continuously monitor the RSSI value in your program, the best way really just depends on your use case. How do you plan the RSSI monitoring?
1. Simplest way to continuously monitor RSSI values is to use connection monitoring. In connection monitoring, you use another chip that continuously monitors the RSSI value between itself and the connected device. This will give you a RSSI value between the main device and the connected device, as well as a stronger RSSI value between the connection monitoring device and the connected device.
Otherwise, you can also subscribe to a Connection event or HCI event. I have outlined both below:
case BLEAPPUTIL_CONN_EVENT_ALL:
{
int rssi_value;
BLEAppUtil_gapConnData_t* connData = (BLEAppUtil_gapConnData_t *) pMsgData;
rssi_value = connData->connEventRpt.lastRssi;
break;
}
case BLEAPPUTIL_HCI_LE_EVENT_CODE:
{
int rssi_value;
hciEvt_BLECteConnectionIqReport_t* hciData = (hciEvt_BLECteConnectionIqReport_t*)pMsgData;
rssi_value = hciData.rssi;
break;
}
Any one of these three methods should work, but if you could provide your use case I can better advice on which one to use. Thanks.
Eshaan
Hi,
I need to read RSSI for the connected device only, I am using BLE as a peripheral device. I am not able to get event BLEAPPUTIL_CONN_EVENT_ALL in code.
I need to continuously monitor the RSSI strength of the connected device, and has to change PHY value as per the RSSI state for fast data transfer.
Hello,
Here is my app_connection.c file, I was able to implement continuous monitoring of rssi values of the connected device.
Important changes to note:
- BLEAPPUTIL_CONN_NOTI_TYPE allows application to receive events for every connection notification, so a separate handler has to be declared to handle this.
BLEAppUtil_EventHandler_t connectionConnNotifyHandler =
{
.handlerType = BLEAPPUTIL_CONN_NOTI_TYPE,
.pEventHandler = Connection_ConnNotifyEventHandler,
.eventMask = BLEAPPUTIL_CONN_NOTI_CONN_ESTABLISHED |
BLEAPPUTIL_CONN_NOTI_PHY_UPDATE |
BLEAPPUTIL_CONN_NOTI_CONN_EVENT_ALL
};
- Since the event you want to use is a Connection Notification, BLE stack uses an additional register function: BLE_registerConnNotiHandler(). I call this in the BLEAPPUTIL_LINK_ESTABLISHED_EVENT case so that notifications are enabled once a connection is formed.
- actual case handling of the event is exactly as I mentioned above, you just need to put it in a different conenction handler function that has to be declared and registered similar to the other ones:
/******************************************************************************
@file app_connection.c
@brief This example file demonstrates how to activate the central role with
the help of BLEAppUtil APIs.
Group: WCS, BTS
Target Device: cc23xx
******************************************************************************
Copyright (c) 2022-2025, Texas Instruments Incorporated
All rights reserved.
Redistribution and use in source and binary forms, with or without
modification, are permitted provided that the following conditions
are met:
* Redistributions of source code must retain the above copyright
notice, this list of conditions and the following disclaimer.
* Redistributions in binary form must reproduce the above copyright
notice, this list of conditions and the following disclaimer in the
documentation and/or other materials provided with the distribution.
* Neither the name of Texas Instruments Incorporated nor the names of
its contributors may be used to endorse or promote products derived
from this software without specific prior written permission.
THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
******************************************************************************
*****************************************************************************/
#if ( HOST_CONFIG & ( CENTRAL_CFG | PERIPHERAL_CFG ) )
//*****************************************************************************
//! Includes
//*****************************************************************************
#include <string.h>
#include <stdarg.h>
#include "ti_ble_config.h"
#include "ti/ble/app_util/framework/bleapputil_api.h"
#include "ti/ble/app_util/menu/menu_module.h"
#include <app_main.h>
//*****************************************************************************
//! Prototypes
//*****************************************************************************
void Connection_ConnEventHandler(uint32 event, BLEAppUtil_msgHdr_t *pMsgData);
void Connection_HciGAPEventHandler(uint32 event, BLEAppUtil_msgHdr_t *pMsgData);
void Connection_ConnNotifyEventHandler(uint32 event, BLEAppUtil_msgHdr_t *pMsgData);
static uint8_t Connection_addConnInfo(uint16_t connHandle, uint8_t *pAddr);
static uint8_t Connection_removeConnInfo(uint16_t connHandle);
//*****************************************************************************
//! Globals
//*****************************************************************************
// Events handlers struct, contains the handlers and event masks
// of the application central role module
BLEAppUtil_EventHandler_t connectionConnHandler =
{
.handlerType = BLEAPPUTIL_GAP_CONN_TYPE,
.pEventHandler = Connection_ConnEventHandler,
.eventMask = BLEAPPUTIL_LINK_ESTABLISHED_EVENT |
BLEAPPUTIL_LINK_TERMINATED_EVENT |
BLEAPPUTIL_LINK_PARAM_UPDATE_EVENT |
BLEAPPUTIL_LINK_PARAM_UPDATE_REQ_EVENT
};
BLEAppUtil_EventHandler_t connectionHciGAPHandler =
{
.handlerType = BLEAPPUTIL_HCI_GAP_TYPE,
.pEventHandler = Connection_HciGAPEventHandler,
.eventMask = BLEAPPUTIL_HCI_COMMAND_STATUS_EVENT_CODE |
BLEAPPUTIL_HCI_LE_EVENT_CODE
};
BLEAppUtil_EventHandler_t connectionConnNotifyHandler =
{
.handlerType = BLEAPPUTIL_CONN_NOTI_TYPE,
.pEventHandler = Connection_ConnNotifyEventHandler,
.eventMask = BLEAPPUTIL_CONN_NOTI_CONN_ESTABLISHED |
BLEAPPUTIL_CONN_NOTI_PHY_UPDATE |
BLEAPPUTIL_CONN_NOTI_CONN_EVENT_ALL
};
// Holds the connection handles
static App_connInfo connectionConnList[MAX_NUM_BLE_CONNS];
//*****************************************************************************
//! Functions
//*****************************************************************************
/*********************************************************************
* @fn Connection_ConnEventHandler
*
* @brief The purpose of this function is to handle connection related
* events that rise from the GAP and were registered in
* @ref BLEAppUtil_registerEventHandler
*
* @param event - message event.
* @param pMsgData - pointer to message data.
*
* @return none
*/
void Connection_ConnEventHandler(uint32 event, BLEAppUtil_msgHdr_t *pMsgData)
{
switch(event)
{
case BLEAPPUTIL_LINK_ESTABLISHED_EVENT:
{
gapEstLinkReqEvent_t *gapEstMsg = (gapEstLinkReqEvent_t *)pMsgData;
bStatus_t status;
// Add the connection to the connected device list
Connection_addConnInfo(gapEstMsg->connectionHandle, gapEstMsg->devAddr);
status = BLEAppUtil_registerConnNotifHandler(gapEstMsg->connectionHandle, GAP_CB_CONN_EVENT_ALL);
//status = BLEAppUtil_registerConnNotifHandler(gapEstMsg->connectionHandle, GAP_CB_CONN_ESTABLISHED);
/*! Print the peer address and connection handle number */
MenuModule_printf(APP_MENU_CONN_EVENT, 0, "Conn status: Established - "
"Connected to " MENU_MODULE_COLOR_YELLOW "%s " MENU_MODULE_COLOR_RESET
"connectionHandle = " MENU_MODULE_COLOR_YELLOW "%d" MENU_MODULE_COLOR_RESET,
BLEAppUtil_convertBdAddr2Str(gapEstMsg->devAddr), gapEstMsg->connectionHandle);
/*! Print the number of current connections */
MenuModule_printf(APP_MENU_NUM_CONNS, 0, "Connections number: "
MENU_MODULE_COLOR_YELLOW "%d " MENU_MODULE_COLOR_RESET,
linkDB_NumActive());
break;
}
case BLEAPPUTIL_LINK_TERMINATED_EVENT:
{
gapTerminateLinkEvent_t *gapTermMsg = (gapTerminateLinkEvent_t *)pMsgData;
// Remove the connection from the conneted device list
Connection_removeConnInfo(gapTermMsg->connectionHandle);
/*! Print the peer address and connection handle number */
MenuModule_printf(APP_MENU_CONN_EVENT, 0, "Conn status: Terminated - "
"connectionHandle = " MENU_MODULE_COLOR_YELLOW "%d " MENU_MODULE_COLOR_RESET
"reason = " MENU_MODULE_COLOR_YELLOW "%d" MENU_MODULE_COLOR_RESET,
gapTermMsg->connectionHandle, gapTermMsg->reason);
/*! Print the number of current connections */
MenuModule_printf(APP_MENU_NUM_CONNS, 0, "Connections number: "
MENU_MODULE_COLOR_YELLOW "%d " MENU_MODULE_COLOR_RESET,
linkDB_NumActive());
break;
}
case BLEAPPUTIL_LINK_PARAM_UPDATE_REQ_EVENT:
{
gapUpdateLinkParamReqEvent_t *pReq = (gapUpdateLinkParamReqEvent_t *)pMsgData;
// Only accept connection intervals with slave latency of 0
// This is just an example of how the application can send a response
if(pReq->req.connLatency == 0)
{
BLEAppUtil_paramUpdateRsp(pReq,TRUE);
}
else
{
BLEAppUtil_paramUpdateRsp(pReq,FALSE);
}
break;
}
case BLEAPPUTIL_LINK_PARAM_UPDATE_EVENT:
{
gapLinkUpdateEvent_t *pPkt = (gapLinkUpdateEvent_t *)pMsgData;
// Get the address from the connection handle
linkDBInfo_t linkInfo;
if (linkDB_GetInfo(pPkt->connectionHandle, &linkInfo) == SUCCESS)
{
// The status HCI_ERROR_CODE_PARAM_OUT_OF_MANDATORY_RANGE indicates that connection params did not change but the req and rsp still transpire
if(pPkt->status == SUCCESS)
{
MenuModule_printf(APP_MENU_CONN_EVENT, 0, "Conn status: Params update - "
"connectionHandle = " MENU_MODULE_COLOR_YELLOW "%d " MENU_MODULE_COLOR_RESET,
pPkt->connectionHandle);
}
else
{
MenuModule_printf(APP_MENU_CONN_EVENT, 0, "Conn status: Params update failed - "
MENU_MODULE_COLOR_YELLOW "0x%x " MENU_MODULE_COLOR_RESET
"connectionHandle = " MENU_MODULE_COLOR_YELLOW "%d " MENU_MODULE_COLOR_RESET,
pPkt->opcode, pPkt->connectionHandle);
}
}
break;
}
default:
{
break;
}
}
}
/*********************************************************************
* @fn Connection_HciGAPEventHandler
*
* @brief The purpose of this function is to handle HCI GAP events
* that rise from the HCI and were registered in
* @ref BLEAppUtil_registerEventHandler
*
* @param event - message event.
* @param pMsgData - pointer to message data.
*
* @return none
*/
void Connection_HciGAPEventHandler(uint32 event, BLEAppUtil_msgHdr_t *pMsgData)
{
switch (event)
{
case BLEAPPUTIL_HCI_COMMAND_STATUS_EVENT_CODE:
{
hciEvt_CommandStatus_t *pHciMsg = (hciEvt_CommandStatus_t *)pMsgData;
switch ( event )
{
case HCI_LE_SET_PHY:
{
if (pHciMsg->cmdStatus ==
HCI_ERROR_CODE_UNSUPPORTED_REMOTE_FEATURE)
{
MenuModule_printf(APP_MENU_CONN_EVENT, 0, "Conn status: Phy update - failure, peer does not support this");
}
else
{
MenuModule_printf(APP_MENU_CONN_EVENT, 0, "Conn status: Phy update - "
MENU_MODULE_COLOR_YELLOW "0x%02x" MENU_MODULE_COLOR_RESET,
pHciMsg->cmdStatus);
}
break;
}
default:
{
break;
}
break;
}
}
case BLEAPPUTIL_HCI_LE_EVENT_CODE:
{
hciEvt_BLEPhyUpdateComplete_t *pPUC = (hciEvt_BLEPhyUpdateComplete_t*) pMsgData;
if (pPUC->BLEEventCode == HCI_BLE_PHY_UPDATE_COMPLETE_EVENT)
{
if (pPUC->status != SUCCESS)
{
MenuModule_printf(APP_MENU_CONN_EVENT, 0, "Conn status: Phy update failure - connHandle = %d",
pPUC->connHandle);
}
else
{
#if !defined(Display_DISABLE_ALL)
char * currPhy =
(pPUC->rxPhy == PHY_UPDATE_COMPLETE_EVENT_1M) ? "1 Mbps" :
(pPUC->rxPhy == PHY_UPDATE_COMPLETE_EVENT_2M) ? "2 Mbps" :
(pPUC->rxPhy == PHY_UPDATE_COMPLETE_EVENT_CODED) ? "CODED" : "Unexpected PHY Value";
MenuModule_printf(APP_MENU_CONN_EVENT, 0, "Conn status: Phy update - connHandle = %d PHY = %s",
pPUC->connHandle, currPhy);
#endif // #if !defined(Display_DISABLE_ALL)
}
}
break;
}
default:
{
break;
}
}
}
void Connection_ConnNotifyEventHandler(uint32 event, BLEAppUtil_msgHdr_t *pMsgData)
{
switch (event) {
case BLEAPPUTIL_CONN_NOTI_CONN_EVENT_ALL:
{
BLEAppUtil_gapConnData_t* connData = (BLEAppUtil_gapConnData_t *) pMsgData;
uint8_t rssi_value;
rssi_value = connData->connEventRpt.lastRssi;
MenuModule_printf(APP_MENU_PROFILE_STATUS_LINE2,0,"current rssi_value: %d", rssi_value);
break;
}
case BLEAPPUTIL_CONN_NOTI_CONN_ESTABLISHED:
{
break;
}
default:
{
break;
}
}
}
/*********************************************************************
* @fn Connection_addConnInfo
*
* @brief Add a device to the connected device list
*
* @return index of the connected device list entry where the new connection
* info is put in.
* If there is no room, MAX_NUM_BLE_CONNS will be returned.
*/
static uint8_t Connection_addConnInfo(uint16_t connHandle, uint8_t *pAddr)
{
uint8_t i = 0;
for (i = 0; i < MAX_NUM_BLE_CONNS; i++)
{
if (connectionConnList[i].connHandle == LINKDB_CONNHANDLE_INVALID)
{
// Found available entry to put a new connection info in
connectionConnList[i].connHandle = connHandle;
memcpy(connectionConnList[i].peerAddress, pAddr, B_ADDR_LEN);
break;
}
}
return i;
}
/*********************************************************************
* @fn Connection_removeConnInfo
*
* @brief Remove a device from the connected device list
*
* @return index of the connected device list entry where the new connection
* info is removed from.
* If connHandle is not found, MAX_NUM_BLE_CONNS will be returned.
*/
static uint8_t Connection_removeConnInfo(uint16_t connHandle)
{
uint8_t i = 0;
uint8_t index = 0;
uint8_t maxNumConn = MAX_NUM_BLE_CONNS;
for (i = 0; i < maxNumConn; i++)
{
if (connectionConnList[i].connHandle == connHandle)
{
// Mark the entry as deleted
connectionConnList[i].connHandle = LINKDB_CONNHANDLE_INVALID;
break;
}
}
// Save the index to return
index = i;
// Shift the items in the array
for(i = 0; i < maxNumConn - 1; i++)
{
if (connectionConnList[i].connHandle == LINKDB_CONNHANDLE_INVALID &&
connectionConnList[i + 1].connHandle == LINKDB_CONNHANDLE_INVALID)
{
break;
}
if (connectionConnList[i].connHandle == LINKDB_CONNHANDLE_INVALID &&
connectionConnList[i + 1].connHandle != LINKDB_CONNHANDLE_INVALID)
{
memmove(&connectionConnList[i], &connectionConnList[i+1], sizeof(App_connInfo));
connectionConnList[i + 1].connHandle = LINKDB_CONNHANDLE_INVALID;
}
}
return index;
}
/*********************************************************************
* @fn Connection_getConnList
*
* @brief Get the connection list
*
* @return connection list
*/
App_connInfo *Connection_getConnList(void)
{
return connectionConnList;
}
/*********************************************************************
* @fn Connection_getConnhandle
*
* @brief Find connHandle in the connected device list by index
*
* @return the connHandle found. If there is no match,
* MAX_NUM_BLE_CONNS will be returned.
*/
uint16_t Connection_getConnhandle(uint8_t index)
{
if (index < MAX_NUM_BLE_CONNS)
{
return connectionConnList[index].connHandle;
}
return MAX_NUM_BLE_CONNS;
}
/*********************************************************************
* @fn Connection_start
*
* @brief This function is called after stack initialization,
* the purpose of this function is to initialize and
* register the specific events handlers of the connection
* application module
*
* @return SUCCESS, errorInfo
*/
bStatus_t Connection_start()
{
bStatus_t status = SUCCESS;
uint8 i;
// Initialize the connList handles
for (i = 0; i < MAX_NUM_BLE_CONNS; i++)
{
connectionConnList[i].connHandle = LINKDB_CONNHANDLE_INVALID;
}
status = BLEAppUtil_registerEventHandler(&connectionConnHandler);
if(status != SUCCESS)
{
return(status);
}
status = BLEAppUtil_registerEventHandler(&connectionHciGAPHandler);
if(status != SUCCESS)
{
return(status);
}
status = BLEAppUtil_registerEventHandler(&connectionConnNotifyHandler);
if (status != SUCCESS)
{
return(status);
}
return status;
}
/*********************************************************************
* @fn Connection_getConnIndex
*
* @brief Find index in the connected device list by connHandle
*
* @return the index of the entry that has the given connection handle.
* if there is no match, LL_INACTIVE_CONNECTIONS will be returned.
*/
uint16_t Connection_getConnIndex(uint16_t connHandle)
{
uint8_t i;
for (i = 0; i < MAX_NUM_BLE_CONNS; i++)
{
if (connectionConnList[i].connHandle == connHandle)
{
return i;
}
}
return LL_INACTIVE_CONNECTIONS;
}
#endif // ( HOST_CONFIG & (CENTRAL_CFG | PERIPHERAL_CFG) )
Thanks!
Eshaan