Part Number: CC2340R5
Other Parts Discussed in Thread: SYSCONFIG
Tool/software:
hi,
When can CC2340R5 support coexistence?
if it already supports, how can I enable 3-wire coexistence?
BR,
frank
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Frank,
Coexistence has been available in the SimpleLink F3 SDK since at least v9.11 and can be configured from SysConfig's RCL module. Documentation is fairly similar to the F2 SDK module but I am working on getting a new version integrated into F3 SDK documents.

Regards,
Ryan
Ryan,
I enable coex in sysconfig.
https://e2e.ti.com/cfs-file/__key/communityserver-discussions-components-files/538/6835.basic_5F00_ble.syscfg
I also add "RCL_GPIO_enable();" in code.
int main()
{
/* Register Application callback to trap asserts raised in the Stack */
halAssertCback = AssertHandler;
RegisterAssertCback(AssertHandler);
Board_init();
RCL_GPIO_enable();
No matter, I set GRANT to high or low. I can still find basic_ble device.
I measure request and priority pin. They are always low.
I miss something?
BR,
frank
What in your view is RCL_GPIO_enable used for? You shouldn't have to add any APIs to the project. GRANT is an input to the CC2340R5, not an output like REQUEST and PRIORITY, as described in this Coexistence Guide. What Coex mode are you using? Perhaps you would get some use out of RF Output Debugging as well.
Regards,
Ryan
Ryan,
I force Grant low\ high to check if coexistence works or not.
I also enable LNA_EN and PA_EN. LNA_EN and PA_EN always has signal no matter GRANT is high or low.

no matter I add "RCL_GPIO_enable();" or not, the result is the same.
Any idea?
BR,
frank
Thanks for the information Frank, I am having a BLE expert test and they will report to you shortly.
Regards,
Ryan
And I do apologize as I've recently found an internal page which insinuates that BLE Coexistence will not be available until SimpleLink F3 SDK v9.20, so the existing Coexistence option may only be intended for IEEE 802.15.4-based solutions (such as Zigbee).
Regards,
Ryan