This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP-EM-CC2340R5: Bluetooth forum

Part Number: LP-EM-CC2340R5

Tool/software:

What is the target impedance for CC2340R52E0RGE on LP-EM-CC2340R5-RGE evaluation board at pin 1 ?

How much is influenced by a 2-layer or 4 layer stack up or number vias in the center pad?

  • Hi Thomas,

    1. The target impedance is 50 ohms at the pin.

    2. Technically, the number layers does not matter as it is the substrate (Between layer 1 and layer 2) thickness and dialectic constant that will have the most impact on impedance, which means thickness = 0.73mm and Er = 4.5.

    3. The number vias will only affect impedance if there are no vias. If you follow the recommend footprint in the datasheet, then there should be no problem.

    Best regards.

    Bun