This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2745R10-Q1: CC2745 program HSM

Part Number: CC2745R10-Q1
Other Parts Discussed in Thread: UNIFLASH

Tool/software:

Hi TI Engineer,

I am currently using an external SWD tool to program the CC2745. I am able to program flash, CCFG, and SCFG. Now I need to program the HSM. According to the official procedure, the .bin file (cc27xxx10_hsm_fw_v3.0.0.bin) is used for the update. However, since this .bin file is encrypted, I am not sure how to use external tools to perform the HSM update or how to parse the file.

We have considered an alternative approach using
simplelink_lowpower_f3_sdk_xx\examples\nortos\LP_EM_CC2745R10_Q1\hsm\hsmfwupdate
to generate an HSM update image and perform the update as follows:

  1. Build an HSM update project image.

  2. Program the image to flash.

  3. Power cycle and run the project to update the HSM.

  4. Erase flash.

  5. Program the application file (including flash/CCFG, etc.).

  6. Verify all programmed memory.

We would like to use the above method to update the HSM, but we are not certain if this approach is valid.

I would like to ask whether it is possible to program the HSM using this method.Or is there an alternative method to update the HSM, such as using the SACI command.

Thank you for your support.

  • Hello,

    • Build an HSM update project image.

    • Program the image to flash.

    • Power cycle and run the project to update the HSM.

    • Erase flash.

    • Program the application file (including flash/CCFG, etc.).

    • Verify all programmed memory.

    This is a valid approach. 

    However, since this .bin file is encrypted, I am not sure how to use external tools to perform the HSM update or how to parse the file.

    Yes, this binary is encrypted, but will be decrypted on the device when loaded. However, if you want to use SACI, you can use the following command flow:

    1. Power up the chip, send SACI_CMD_MISC_NO_OPERATION with a sequence number of something >  1 (It can be zero, but it may be better to start with a number > 0).
      1. Verify that the command was success by reading the response, and verify that the sequence number matches what was sent
    2. SACI_CMD_FLASH_VERIFY_MAIN_SECTORS
      1. If the flash is not blank proceed to 3.
    3. SACI_CMD_FLASH_ERASE_CHIP
    4. SACI_CMD_PROG_MAIN_PIPELINED
    5. SACI_CMD_FLASH_PROG_CCFG_SECTOR
    6. SACI_CMD_FLASH_VERIFY_CCFG_SECTOR
    7. SACI_CMD_FLASH_PROG_SCFG_SECTOR
    8. SACI_CMD_FLASH_VERIFY_SCFG_SECTOR
    9. SACI_CMD_BLDR_APP_RESET_DEVICE
      1. We must reset before provisioning the HSM FW.
    10. SACI_CMD_MISC_NO_OPERATION (repeat step 1)
      1. Verify that the command was success by reading the response, and verify that the sequence number matches what was sent
      2. If it was not successful, then SACI communication is not ready.
    11. SACI_CMD_HSM_FW_PROVISION

    Please let me know if this works for you!

    Best,

    Nima Behmanesh

  • Hi Nima,

    Thank you for your reply. I am now trying to use the SACI procedure you provided to program the HSM. I sent the data from cc27xxx10_hsm_fw_v3.0.0.bin (length 0x13640)into the CC2745 using the SACI_CMD_HSM_FW_PROVISION (HUI DATA). After execution, I received the message HSM_FW_VER_INVALID, but I do not understand what this means.

    Afterwards, I read the HSM information and obtained the version number 4.5.7. I would like to confirm with you whether my procedure is correct, and how I can resolve the HSM_FW_VER_INVALID message.

    In addition, may I ask if there is any way to verify the HSM after programming, or is checking the version number the only method?

    Best regards,

    Harry

  • Hello,

    Let me reach out to R&D. Please allow me some time to get feedback.

    Best,

    Nima Behmanesh

  • Hello,

    After reaching out to R&D, can you verify that before you do the procedure that the device is blank (including that there is no HSM firmware on the device)?

    This can be done by doing two back-to-back chip erases. Additionally, before running the procedure you can read the HSM firmware version. If a version is replied back, then the chip is not blank.

    Best,

    Nima Behmanesh

  • Hi Nima,

    I have resolved the issues mentioned above. I have now confirmed that SACI_CMD_HSM_FW_PROVISION executed successfully.

    I have a question: After completing the above procedure, I tried using SACI_CMD_GET_SECBOOT_HSMFW_UPDATE_STATUS and received the result STATUS_INVALID_SB_CONFIG (0x6): Secure Boot configuration is invalid.

    Could you please advise whether this will have any impact, or can it be ignored?

    Thanks for your help.

    Best regards,

    Harry

  • Hi Nima,

    Excuse me, I would like to ask: After programming the HSM, I used SACI_CMD_GET_SECBOOT_HSMFW_UPDATE_STATUS and got the status STATUS_INVALID_SB_CONFIG (0x6): Secure Boot configuration is invalid. Will this cause any impact?

    Best regards,

    Harry

  • Hello,

    Are you using Secure Boot? If not then I don't believe this will have any impact.

    Best,

    Nima Behmanesh

  • Hi Nima,

    Thank you for your reply,I would like to ask if this type of error message is normal, or if there is a way to resolve this issue. Since I am using the official code for programming, I am not sure whether secure boot will be used in the future.

  • Hi Nima,

    Since our customer is still waiting for a response, we would like to know the risks associated with STATUS_INVALID_SB_CONFIG (0x6) as well as possible solutions to address it.
    Thank you again for your support.

    Best regards,

    Harry

  • Hi Nima,

    I tried using XDS110 and Uniflash to perform verification on the CC2745, but I encountered the error message: "Target did not enter SACI after pin reset."
    Could you please advise how to resolve this issue? Thank you.

    Best regards,

    Harry

  • Hello,

    Is this an XDS110ET or and XDS110?

    What version of Uniflash are you using? 

    Is there a valid image on the CC2745?

    Do you mind attaching a screenshot of the error?

    Best,

    Nima Behmanesh

  • Hi Nima,

    1. I would first like to know if there is any solution for STATUS_INVALID_SB_CONFIG (0x6) in order to avoid potential impacts on the IC.

    2. I am currently using the web version of Uniflash 9.3.0.5423 with the XDS110 Debug Probe. I am able to read the memory of the CC2745, but when performing other operations, I encounter error messages.

    Best regards,

    Harry

  • . Since I am using the official code for programming, I am not sure whether secure boot will be used in the future.

    This error code is dependent on whether you are using Secure Boot.

    Since you're not using secure boot, and you are using SACI commands to update the HSM firmware (not ROM) then you should be using:
    SACI_CMD_HSM_GET_SYS_ INFO.

    Otherwise, if you are using the ROM APIs and using Secure Boot then you can use:
    SACI_CMD_GET_SECBOOT_ HSMFW_UPDATE_STATUS

    Please try using SACI_CMD_HSM_GET_SYS_INFO instead of SACI_CMD_GET_SECBOOT_HSMFW_UPDATE_STATUS since you're not currently using secure boot.

    I am currently using the web version of Uniflash 9.3.0.5423 with the XDS110 Debug Probe. I am able to read the memory of the CC2745, but when performing other operations, I encounter error messages.

    What other operations are you using that you are seeing errors?

    Best,

    Nima Behmanesh

  • Hello Nima,

    Thank you for your reply.
    When I try to use functions such as "Perform Blank Check" or "Read HSM Info", I always get an error.
    Only "Read Memory" and "Reset" work correctly.
    It seems that any function requiring SACI commands results in this error message.

    Best regards,

    Harry