Part Number: CC2340R5
Other Parts Discussed in Thread: UNIFLASH,
Tool/software:
Hi,
I am Facing error 614 in programing c2340 mcu what should i do to resolve it

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi akash,
The error indicates that the XDS110 is connected to the computer properly, are you using LP-EM-CC2340R5 hardware as a target? Make sure that the TGT VDD header on the XDS110 selects XDS so long as you are planning to power the board through the XDS110 hardware. Have you successfully programmed this hardware before? Have you tried using UNIFLASH instead of CCS?
Regards,
Ryan
Hi Ryan,
I am working with a custom board, which I had successfully programmed multiple times for debugging. However, the error suddenly started occurring. I have also attempted to clear the flash serially and reprogram the device, but the error persists. i
What tools are you using, and have you tried both CCS and Uniflash to clear device memory? What is the CC2340R5 version from the device info in your Uniflahs Settings & Utilities? What version of the SimpleLink F3 SDK are you using? If the JTAG SWO interface has somehow been locked then you may try to erase and correct the device through the TI_CC2340_Linux_SBL assuming the CCFG is using FCFG settings for the bootloader.

Regards,
Ryan
Yes, I have tried both UniFlash and CCS to clear the device memory, but the same error occurs in both cases. My CC2340R5 device is Revision C (2.1). As you mentioned, I also attempted to erase and recover the device, but the issue still persists.
Besides the ROM serial bootloader option, I recommend you submit your design to SIMPLELINK-2-4GHZ-DESIGN-REVIEWS so that the custom hardware may be reviewed and further JTAG locks are avoided.
You can also search for other E2E resolutions and determine whether any suggestions work in your setup. Below are examples but not a thorough search:
CC2340R5: JTAG Communication during programming
LP-EM-CC2340R5: Unlock PG2.0 chip - suggested steps give error
Regards,
Ryan