CC2340R2: Functions Missing in 9.12

Expert 3880 points
Part Number: CC2340R2

Tool/software:

Hi,

The 4 functions below were defined in the hci.h header file for SDK 8.40.00.61, but are not in 9.12.00.19. Are they no longer supported or did the function names change?

Warning[Pe223]: function "HCI_EXT_SetFreqTuneCmd" declared implicitly      

Warning[Pe223]: function "HCI_EXT_HaltDuringRfCmd" declared implicitly     

Warning[Pe223]: function "HCI_EXT_SaveFreqTuneCmd" declared implicitly   

Warning[Pe223]: function "HCI_EXT_ExtendRfRangeCmd" declared implicitly

Best,

Luke

  • Hi Luke,

    I am not sure if these functions were supported in the F3 SDK. It is possible they were non-working and fully removed in the 9.12 SDK. Were you able to use these functions in a previous F3 SDK release succesfully?

    Best Regards,

    Jan

  • Hi Jan, 

    This was my assumption as well. Customer does not appear to be using these previously and were just checking for CM testing purposes.

    Thanks,

    Luke