Tool/software:
Hi,
I am using TI Zephyr fork v3.7.0-ti-8.40.00_ea (https://github.com/TexasInstruments/simplelink-zephyr/tree/v3.7.0-ti-8.40.00_ea) for the target evaluation board LP_EM_CC2340R53.
My project involves C++ sources, however when I try to enable support for C++; the project does not boot-up.
In order to experiment further, I try to build the peripheral example and enabled support for C++ by adding the KConfig macro in the prj.conf file
-- west build: generating a build system Loading Zephyr default modules (Zephyr base). -- Application: C:/Users/ekb6fe/simplelink_zephyr/zephyr/samples/bluetooth/peripheral -- CMake version: 4.0.3 -- Found Python3: C:/Users/ekb6fe/simplelink_zephyr/.venv/Scripts/python.exe (found suitable version "3.13.7", minimum required is "3.8") found components: Interpreter -- Cache files will be written to: C:/Users/usr/simplelink_zephyr/zephyr/.cache -- Zephyr version: 3.7.0 (C:/Users/usr/simplelink_zephyr/zephyr) -- Found west (found suitable version "1.4.0", minimum required is "0.14.0") -- Board: lp_em_cc2340r53, qualifiers: cc2340r53 -- Found host-tools: zephyr 0.16.8 (C:/usr/ekb6fe/zephyr-sdk-0.16.8) -- Found toolchain: zephyr 0.16.8 (C:/usr/ekb6fe/zephyr-sdk-0.16.8) -- Found Dtc: C:/Users/usr/AppData/Local/Microsoft/WinGet/Packages/oss-winget.dtc_Microsoft.Winget.Source_8wekyb3d8bbwe/usr/bin/dtc.exe (found suitable version "1.6.1", minimum required is "1.4.6") -- Found BOARD.dts: C:/Users/usr/simplelink_zephyr/zephyr/boards/ti/lp_em_cc2340r53/lp_em_cc2340r53.dts -- Generated zephyr.dts: C:/usr/ekb6fe/simplelink_zephyr/build/app/zephyr/zephyr.dts -- Generated devicetree_generated.h: C:/Users/usr/simplelink_zephyr/build/app/zephyr/include/generated/zephyr/devicetree_generated.h