CC2642R: BLE SDK upgrade from 3.10.00.53 to 3.40.00.02, sleep base current abnormal

Part Number: CC2642R
Other Parts Discussed in Thread: SYSCONFIG

Hi,

I just upgraded my CC2642 project SDK from 3.10.00.53 to 3.40.00.02. In 3.40.00.02, the peripheral configurations are edited by Sysconfig tools. I edited the syscfg file and implement the peripheral settings the same as used to in SDK 3.10.00.53. 

In low power mode, UART and SPI are disabled, only with a 50ms ADV, I find that the sleep base current with a about 10ms periodical abnormal signal, average current about 8.4 uA and max to 24uA. There is no any 10ms periodical tasks in my project yet. 

Is there any other special settings? or the new SDK was running some new features?

 

while in SDK 3.10.00.53 the sleep base current is much flatter,  average current about 1.6 uA