Part Number: CC2642R
Hi.
Chip model: CC2642
SDK ver: simplelink_cc13xx_cc26xx_sdk_7_41_00_17
I would like to ask if it is possible for the following situations to occur when connecting the CC2642 to a mobile phone
An IOS phone connects to the CC2642 and sends data to it. Once, the phone sent A packet of data A to the CC2642, but the protocol stack did not notify the application layer to read it. When the phone sent data B to the CC2642 again, the protocol stack informed the application layer to read it, but the data read was the previous data A.
Once this situation occurs, even if the Bluetooth is disconnected and the connection is reconnected, when the mobile phone sends data to the CC2642 and the protocol stack notifies the application layer to read it, the obtained data is still the old data that was not notified before the disconnection .
Trouble reply as soon as .
Thank you!