This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2540 Data Throughput Data Rate

Other Parts Discussed in Thread: CC2540

According to the Bluetooth SIG, BR is about 60% faster than LE for large data transfers.

That is, a 1MB transfer on BR takes about 8.81seconds and the same over LE takes about 13.93 seconds.

I am using the HostTestRelease-USB in conjunction with the ble\Thermometer project on the KeyFOB.

On modifying the ble\Thermometer project to accept ReadBlob accesses, I found that in a large transfer, each packet (of 22bytes) is transferred roughly every 200ms.

This works out at about 9000 seconds for a 1MB transfer or about 650 times slower than the Bluetooth SIG information.

It is obvious that the 200ms is some artificial limitation, but I don't know where to start looking.

Has anybody looked into LE throughput on the CC2540? Is there any example code anywhere?

Thanks

Karel