Part Number: CC2340R5-Q1
Other Parts Discussed in Thread: CC2340R5
Hi team
My customer steel mate has some problem:
The Iron General (a Chinese electronics company) has a project called "Great Yangtze" that requires the CC2340R5 chip. The requirement is to use the CC2340R5 as a BLE Bluetooth slave, connecting to a mobile app via the HID protocol and communicating with the MCU via serial port. Since I am unfamiliar with this chip, I have the following questions:
1. Based on the above requirements, which SDK version would you recommend? Which operating system, TIrtos or Freertos, would be more suitable and reliable? Which example code would be easier to use for development?
2. Does it support the HID protocol? Are there any example codes I can refer to?
3. Has the chip's MAX address been assigned, and can its uniqueness be guaranteed?