I have several questions regarding the CC2564/CC2560/CC2560A:
(1) Is it correct to assume that the MSP430BT5190 will support the CC2564 or a "new" MSP will be required for such purposes?
(2) If the assumption in (1) is correct, what type of changes will be expected for the firmware in the MSP430BT5190? Specifically, lets say I develop a product with the MSP430BT5190 and the CC2560 now, there is an easy migration path to then use the CC2564?
(3) Is the CC2560A replacing the CC2560? According to the documentation in the Panasonic web site there is a CC2560A with an additional 0.5 dBm of output power as the key difference to the CC2560.
(4) Will the dual-mode implementation claimed by Panasonic in their modules utilizing the CC2564 be such that in a piconet Bluetooth Classic and Bluetooth Low Energy devices will inter-operate?
(5) So far, Panasonic is publishing the availability of the CC2564 and its operation with the MSP. When can I expect TI's strategy to these two devices?
Thanks in advance,
-Manuel