Part Number: WL18XX-REPORTS
Our system is an industrial IoT gateway which uses a WL1871 (packaged as Jorjin WG7871-BN). As of December of 2024, the some gateways deployed in the field started experiencing HCI timeouts that were not recoverable via a chip reset.
We were able to replicate the issue in the lab while capturing the BT FW logs, an HCI dump on the gateway and a trace of over the air traffic using a sniffer. After configuring the BT chip, an LE scan is started. A few devices are reported in the scan, but then:
7626656 11/13/25 17:07:30.486 -0:00:24.421 OSA_BUF_Exception called with code: 65535 - OSA_BUF_ERROR_CORRUPTED
...
7626736 11/13/25 17:07:30.516 -0:00:24.391 ERROR: Hard Fault Exception in MAIN MCU. Details follows: **************************************