This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2340R5: LP-EM-CC2340R53: car_node Example Stuck in Assert Handler (OUT_OF_MEMORY)

Part Number: CC2340R5
Other Parts Discussed in Thread: SYSCONFIG,

Hello,

I’ve tested the car_node example on the LP-EM-CC2340R53 board, and the program gets stuck in the assert handler due to an OUT_OF_MEMORY error. After checking the memory usage, the remaining free heap is only 80 bytes.

SDK Version: 9.14.01.16
Board: LP-EM-CC2340R53

The example was flashed directly to the development board without any modifications.

Does this example require any specific code configuration?

Thank you.

 

 

Screenshot from 2026-01-13 08-51-34.png