Other Parts Discussed in Thread: CC2540, CC2530
Hello all,
For my application, I need on one side to handle the CC2540USB Master (HostTestRelease) on a Linux distribution, and on the other side, to handle it in slave configuration using a microcontroller such as an msp430 to communicate over HCI layer using physical SPI.
I noticed that the current TI BLE stack does not support "LE only commands". For the moment, it worked with the "HCI vendor specific commands". I didn't try the other type for the moment but I suppose that it works too. However, I saw that LE commands may be working with the future version of the TI BLE stack. Same concerning the SPI support.
- Does anyone have more information about the release date of the 1.2 version? Or some news about “LE only commands” and SPI support?
- Is there any project around using an msp430 with the CC2540?
Thanks a lot for your help,
CS